JAJSL38 December 2023 TPSI3100-Q1
ADVANCE INFORMATION
The TPSI310x-Q1 and TPSI313x-Q1 devices include one alarm comparator. The TPSI312x-Q1 devices include two alarm comparators. An alarm comparator differs from the fault comparator in that the output state of the comparator has no direct control of the VDRV output driver. The block diagram of the alarm comparator is shown in Figure 8-8.
If the input voltage of the alarm comparator, ALM1_CMP, exceeds the internal reference voltage, VREF, the comparator output asserts high. The comparator output is filtered and is adjustable via an external 1% resistor, RRESP, connected from RESP to VSSS. The filtering of low-to-high transitions of the comparator output is adjustable by the external resistor. High-to-low transitions of the comparator output are filtered at a fixed setting. The filter setting is shared by both the fault and alarm comparators and cannot be set independently. In addition, the alarm comparator is not latched.
Similar to the fault comparator, the alarm comparator output information is transferred to the primary side of the device via back-channel communication (BCC) over the isolation barrier. As shown in Figure 8-8, any low-to-high transition of the comparator output (alarm event) that passes through the filter is extended to make sure the event is captured by the sample logic. Any high-to-low transition of the comparator output (recovery event) that passes through the filter are not extended. A recovery event can be missed by the sample logic if the event does not last longer than the sample period. Therefore, priority is given to alarm events over recovery events. ALM1 open-drain output is asserted low upon the alarm event. If a recovery event occurs and is captured by the sample logic, ALM1 open-drain output is set to high-impedance.