JAJSUQ8D June 2024 – December 2024 TPSM81033
PRODUCTION DATA
There are two ways to set the output voltage of the TPSM81033: adjustable or fixed. If the FB is connected to AVIN, the TPSM81033 works as a fixed 5.0V output voltage version, the TPSM81033 uses the internal resistor divider.The load regulation performance is optimized with the the internal resistor divider.
The output voltage is also can be set by an external resistor divider (R1, R2 in Figure 7-1). When the output voltage is regulated, the typical voltage at the FB pin is VREF. Thus the resistor divider is determined by Equation 5.
where