JAJSEZ8A July 2017 – March 2018 TPSM82480
PRODUCTION DATA.
For values up to 0.6V, an external voltage, connected to the SS/TR pin, drives the voltage level at the FB pin. In doing so, the voltage at the FB pin is directly proportional to the voltage at the SS/TR pin.
When choosing the resistive divider proportion according to Equation 8, VOUT tracks VTR simultaneously.
space
space
space
Following the example of Setting the Adjustable Output Voltage with VOUT = 1.8 V, R1 = 240 kΩ and R2 = 120 kΩ, Equation 9 and Equation 10 calculate R3 and R4, connected to the SS/TR pin. Different to the resistive divider at the FB pin, a larger current must be chosen, to avoid a tracking offset caused by the 5.25 µA current that flows out of the SS/TR pin. Assuming a 250 µA current, R4 calculates as follows:
space
space
R3 calculates now rearranging Equation 8:
space
space
However, the following limitations can influence the tracking accuracy: