JAJSNW0D July 2023 – June 2024 TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15
PRODUCTION DATA
If the user changes the output voltage setpoint while the device is operating, the device ramps up or down to the new voltage setting in a controlled way.
The VRAMP[1:0] bits in the CONTROL1 register set the slew rate when the device ramps from one voltage to another during DVS (see Table 7-4). The ramp rate is independent of the setting of the VRANGE[1:0] bits.
| VRAMP[1:0] | DVS Slew Rate |
|---|---|
| 0b00 | 10 mV/μs |
| 0b01 | 5 mV/μs |
| 0b10 (default) | 1.25 mV/μs |
| 0b11 | 0.5 mV/μs |
Note that ramping the output to a higher voltage requires additional output current, so that during DVS the converter must generate a total output current given by:

where:
For correct operation, make sure that the total output current during DVS does not exceed the rated current of the device.