SBAS484B September 2010 – December 2016 TSC2014
PRODUCTION DATA.
TSC2014 should be clean and well-bypassed. A 0.1-μF ceramic bypass capacitor should be added between (VDD/REF and GND). This capacitor must be placed as close to the device as possible. A 1-μF to 10-μF capacitor may also be needed if the impedance of the connection between VDD/REF and the power supply is high.