SLLSE80B March 2011 – June 2015 TUSB1211
PRODUCTION DATA.
The TUSB1211 device is optimized to be interfaced through a 12-pin SDR UTMI Low Pin Interface (ULPI), supporting both input clock and output clock modes, with 1.8 V interface supply voltage. The TUSB1211 device integrates a 3.3-V LDO, which makes it flexible to work with either battery operated systems or pure 3.3-V supplied systems. Both the main supply and the 3.3-V power domain can be supplied through an external switched-mode converter for optimized power efficiency.
The TUSB1211 device includes a POR circuit to detect supply presence on VBAT and VDDIO pins. The TUSB1211 device can be disabled or configured in low power mode for energy saving.
The TUSB1211 device is protected against accidental shorts to 5 V or ground on its exposed interface (DP/DM/ID). It is also protected against up to 20-V surges on VBUS.
The TUSB1211 device also supports the OTG (Ver1.3) optional addendum to the USB2.0 specification, including host negotiation protocol (HNP) and session request protocol (SRP).
The TUSB1211 device integrates a high-performance low-jitter 480-MHz PLL and supports two clock configurations. Depending on the required link configuration, the TUSB1211 device supports both ULPI input and output clock mode: input clock mode, in which case a square-wave 60-MHz clock is provided to TUSB1211 at the ULPI interface CLOCK pin; and output clock mode in which case the TUSB1211 device can accept a square-wave reference clock at REFCLK of either 19.2 MHz or 26 MHz. Frequency is indicated to the TUSB1211 device through the configuration pin CFG, which can be useful if a reference clock is already available in the system.
The on-the-go (OTG) block integrates two main functions:
Four VBUS comparators permit detection of four VBUS levels as described in Table 5-1.
VBUS COMPARATOR | DETECTION STATUS BIT | DETECTION BIT LOGIC |
---|---|---|
VA_VBUS_VLD | VBUSVALID | VBUSVALID = 1 if VBUS > VA_VBUS_VLD else 0 |
VSESS_VLD | SESSVALID | SESSVALID = 1 if VBUS > VSESS_VLD else 0 |
VB_SESS_VLD | BVALID_STS | BVALID_STS = 1 if VBUS > VB_SESS_VLD else 0 |
VB_SESS_END | SESSEND | SESSEND = 0 if VBUS > VB_SESS_END else 1 |
The TUSB1211 device includes a universal serial bus (USB) on-the-go (OTG) transceiver that supports USB 480-Mb/s high-speed (HS), 1-Mb/s full-speed (FS), and USB 1.5-Mb/s low-speed (LS) through a
12-pin UTMI+ low pin interface (ULPI).
NOTE
LS device mode is not allowed by a USB2.0 HS capable PHY, therefore it is not supported by the TUSB1211 device. This is clearly stated in USB2.0 standard Chapter 7, page 119, second paragraph: “A high-speed capable upstream facing transceiver must not support low-speed signaling mode..” There is also some related commentary in Chapter 7.1.2.3.
IO INTERFACE | INTERFACE DESIGNATION | TARGET FREQUENCY | |
---|---|---|---|
USB | Universal serial bus | High speed | 480 Mbits/s |
Full speed | 12 Mbits/s | ||
Low speed | 1.5 Mbits/s |
The PHY is the physical signaling layer of the USB 2.0. It essentially contains all the drivers and receivers required for physical data and protocol signaling on the DP and DM lines.
The PHY interfaces to the USB controller through a standard 12-pin digital interface called UTMI+ low pin interface (ULPI).
The transmitters and receivers inside the PHY are classified into two main classes.
To bias the transistors and run the logic, the PHY also contains reference generation circuitry which consists of:
Built-in pullup and pulldown resistors are used as part of the protocol signaling.
Apart from this, the PHY also contains circuitry which protects it from accidental short on the DP and DM lines to 5 V or GND.
In addition to the differential receiver, there is a single-ended receiver (SE–, SE+) for each of the two data lines DP/–. The main purpose of the single-ended receivers is to qualify the DP and DM signals in the full-speed/low-speed modes of operation.
A differential input receiver (Rx) retrieves the LS/FS differential data signaling. The differential voltage on the line is converted into digital data by a differential comparator on DP/DM. This data is then sent to a clock and data recovery circuit that recovers the clock from the data. An additional serial mode exists in which the differential data is directly output on the RXRCV pin.
The USB transceiver (Tx) uses a differential output driver to drive the USB data signal DP/– onto the USB cable. The driver’s outputs support 3-state operation to achieve bidirectional half-duplex transactions.
The HS receiver consists of the following blocks:
PARAMETER | TEST CONDITIONS | MIN | TYP | MAX | UNIT | |
---|---|---|---|---|---|---|
VHSSQ | High-speed squelch detection threshold (differential signal amplitude) | Ref. USB2.0 | 100 | 150 | mV | |
VHSDSC | High-speed disconnect detection threshold (differential signal amplitude) | Ref. USB2.0 | 525 | 625 | mV | |
High-speed differential input signaling levels | Ref. USB2.0, specified by eye pattern templates | mV | ||||
VHSCM | High-speed data signaling common mode voltage range (guidelines for receiver) | Ref. USB2.0 | –50 | 500 (1) | mV | |
Receiver jitter tolerance | Ref. USB2.0, specified by eye pattern templates | 150 | ps |
The HS transmitter is always operated through the ULPI parallel interface. The parallel data on the interface is serialized, bit stuffed, NRZI encoded, and transmitted as a dc output current on DP or DM depending on the data. Each line has an effective 22.5-Ω load to ground, which generates the voltage levels for signaling.
A disconnect detector is also part of the HS transmitter. A disconnect on the far end of the cable causes the impedance seen by the transmitter to double thereby doubling the differential amplitude seen on the DP/DM lines.
Asserting AUTORESUME bit enables the PHY to automatically transmit resume signaling.
Refer to USB2.0 specification Section 7.1.7.7 and Section 7.9 for more details. When autoresume is enabled, if the PHY detects a resume-K it takes automatically over-driving of the resume-K within 1 ms.
If AUTORESUME_WDOG_EN bit is set (default is 1), then an internal autoresume watchdog timer, based on the internal 32K oscillator, CK32K, will be initialized and will start counting when the PHY detects a resume-K.
If AUTORESUME_WDOG_EN bit is set then if the PHY does not receive a TXCMD of the NOPID type within TAUTORESUME it will stop driving the resume-K and the USB bus will go back to IDLE-J state Otherwise the PHY will continue to drive the resume-K until it receives a TXCMD of the NOPID type from the LINK.
By setting CARKITMODE bit in IFC_CTRL register, the TUSB1211 device will enter UART mode. In this mode, the ULPI data bus is redefined as a 2-pin UART interface, which exchanges data through a direct access to the FS/LS analog transmitter at DM pin and receiver at DP pin. See Figure 5-1 for the USB UART data flow.
Four ID comparators permit detection of five external ID resistances as described in Table 5-4.
EXTERNAL RID DETECTED | DETECTION STATUS BIT | DETECTION BIT LOGIC (DETECTION IF COMP1 < RID < Comp2) |
COMP1 | COMP2 |
---|---|---|---|---|
RID_FLOAT | ID_FLOAT_STS | ID_FLOAT_STS = 1 if (ID_R_ID_A_TO_FLOAT < RID ) else 0 | ID_R_ID_A_TO_FLOAT | — |
RID_A | ID_RARBRC_STS<1:0> | ID_RARBRC_STS<1:0> = "11" if (ID_R_ID_B_TO_A < RID < ID_R_ID_A_TO_FLOAT) else 0 | ID_R_ID_B_TO_A | ID_R_ID_A_TO_FLOAT |
RID_B | ID_RARBRC_STS<1:0> | ID_RARBRC_STS<1:0> = "10" if (ID_R_ID_C_TO_B < RID < ID_R_ID_B_TO_A) else 0 | ID_R_ID_C_TO_B | ID_R_ID_B_TO_A |
RID_C | ID_RARBRC_STS<1:0> | ID_RARBRC_STS<1:0> = "01" if (ID_R_ID_GND_TO_C < RID < ID_R_ID_C_TO_B) else 0 | ID_R_ID_GND_TO_C | ID_R_ID_C_TO_B |
RIDGND | IDGND | IDGND = 0 if (RID < ID_R_ID_GND_TO_C) else 1 | — | ID_R_ID_GND_TO_C |
In order to support Battery Charging Specification v1.1 April 2009 [BCS v1.1], a charger detection module is included inside the TUSB1211 module.
This feature includes:
The detection mechanism aims at distinguishing several types of power sources that can be connected on VBUS line:
Hardware includes:
ID pin status detection (as defined per OTG v1.3 standard as well as ACA resistor types as described in BCS v1.1) and DP/DM Single-Ended receivers (as defined per USB v2.0 standard) are also used to determine the type of device plugged on USB connector.
USB charger detection is an independent feature, on VBAT supply domain, using CK32K clock.
There are 3 modes of operation of battery charger detection module:
Accessory Charger Adapter (ACA) feature is defined in the USB Battery Charging Specification Rev. 1.1 specification. ACA allows simultaneous connection of a USB Charger or Charging Downstream Port and an Accessory to a portable OTG device (TUSB1211).through only a single USB OTG port.
ADDRESS OFFSET | 0x00 | ||
PHYSICAL ADDRESS | 0x00 | INSTANCE | USB_SCUSB |
DESCRIPTION | Lower byte of vendor ID supplied by USB-IF (TI Vendor ID = 0x0451) | ||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
VENDOR_ID |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | VENDOR_ID | R | 0x51 |
ADDRESS OFFSET | 0x01 | ||
PHYSICAL ADDRESS | 0x01 | INSTANCE | USB_SCUSB |
DESCRIPTION | Upper byte of vendor ID supplied by USB-IF (TI Vendor ID = 0x0451) | ||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
VENDOR_ID |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | VEN DOR_ID | R | 0x04 |
ADDRESS OFFSET | 0x02 | ||
PHYSICAL ADDRESS | 0x02 | INSTANCE | USB_SCUSB |
DESCRIPTION | Lower byte of Product ID supplied by Vendor (SAUSB Product ID is 0x1508). | ||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PRODUCT_ID |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | PRODUCT_ID | R | 0x08 |
ADDRESS OFFSET | 0x03 | ||
PHYSICAL ADDRESS | 0x03 | INSTANCE | USB_SCUSB |
DESCRIPTION | Upper byte of Product ID supplied by Vendor (SAUSB Product ID is 0x1508). | ||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PRODUCT_ID |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | PRODUCT_ID | R | 0x15 |
ADDRESS OFFSET | 0x04 | ||
PHYSICAL ADDRESS | 0x04 | INSTANCE | USB_SCUSB |
DESCRIPTION | Controls UTMI function settings of the PHY. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | SUSPENDM | RESET | OPMODE | TERMSELECT | XCVRSELECT |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET | |
---|---|---|---|---|---|
7 | Reserved | R | 0 | ||
6 | SUSPENDM | Active low PHY suspend. Put PHY into Low Power Mode. In Low Power Mode the PHY power down all blocks except the full speed receiver, OTG comparators, and the ULPI interface pins. The PHY automatically set this bit to '1' when Low Power Mode is exited. | RW | 1 | |
5 | RESET | Active high transceiver reset. Does not reset the ULPI interface or ULPI register set. | RW | 0 | |
Once set, the PHY asserts the DIR signal and reset the UTMI core. When the reset is completed, the PHY de-asserts DIR and clears this bit. After de-asserting DIR, the PHY re-assert DIR and send an RX command update. | |||||
Note: This bit is auto-cleared, this explain why it can't be read at '1'. | |||||
4:03 | OPMODE | Select the required bit encoding style during transmit | RW | 0x0 | |
0x0: | Normal operation | ||||
0x1: | Non-driving | ||||
0x2: | Disable bit-stuff and NRZI encoding | ||||
0x3: | Reserved (No SYNC and EOP generation feature not supported) | ||||
2 | TERMSELECT | Controls the internal 1.5 kΩ pullup resistor and 45 Ω HS terminations. Control over bus resistors changes depending on XcvrSelect, OpMode, DpPulldown and DmPulldown. | RW | 0 | |
1:0 | XCVRSELECT | Select the required transceiver speed. | RW | 0x1 | |
0x0: | Enable HS transceiver | ||||
0x1: | Enable FS transceiver | ||||
0x2: | Enable LS transceiver | ||||
0x3: | Enable FS transceiver for LS packets | ||||
(FS preamble is automatically pre-pended) |
ADDRESS OFFSET | 0x05 | ||
PHYSICAL ADDRESS | 0x05 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the func_ctrl register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | SUSPENDM | RESET | OPMODE | TERMSELECT | XCVRSELECT |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | SUSPENDM | RW | 1 | |
5 | RESET | RW | 0 | |
4:3 | OPMODE | RW | 0x0 | |
2 | TERMSELECT | RW | 0 | |
1:0 | XCVRSELECT | RW | 0x1 |
ADDRESS OFFSET | 0x06 | ||
PHYSICAL ADDRESS | 0x06 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the func_ctrl register with read/clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | SUSPENDM | RESET | OPMODE | TERMSELECT | XCVRSELECT |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | SUSPENDM | RW | 1 | |
5 | RESET | RW | 0 | |
4:3 | OPMODE | RW | 0x0 | |
2 | TERMSELECT | RW | 0 | |
1:0 | XCVRSELECT | RW | 0x1 |
ADDRESS OFFSET | 0x07 | ||
PHYSICAL ADDRESS | 0x07 | INSTANCE | USB_SCUSB |
DESCRIPTION | Enables alternative interfaces and PHY features. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
INTERFACE_PROTECT_DISABLE | INDICATORPASSTHRU | INDICATORCOMPLEMENT | AUTORESUME | CLOCKSUSPENDM | CARKITMODE | FSLSSERIALMODE_3PIN | FSLSSERIALMODE_6PIN |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | INTERFACE_PROTECT_DISABLE | Controls circuitry built into the PHY for protecting the ULPI interface when the link tri-states stp and data. | RW | 0 |
0b: Enables the interface protect circuit | ||||
1b: Disables the interface protect circuit | ||||
6 | INDICATORPASSTHRU | Controls whether the complement output is qualified with the internal vbusvalid comparator before being used in the VBUS State in the RXCMD. | RW | 0 |
EXTERNALVBUSINDICATOR input signal is the FAULT input pin of TUSB1211. | ||||
0b: Complement output signal is qualified with the internal VBUSVALID comparator. | ||||
1b: Complement output signal is not qualified with the internal VBUSVALID comparator. | ||||
5 | INDICATORCOMPLEMENT | Tells the PHY to invert EXTERNALVBUSINDICATOR input signal, generating the complement output. | RW | 0 |
EXTERNALVBUSINDICATOR input signal is the FAULT input pin of TUSB1211. | ||||
0b: PHY will not invert signal EXTERNALVBUSINDICATOR (default) | ||||
1b: PHY will invert signal EXTERNALVBUSINDICATOR | ||||
4 | AUTORESUME | Enables the PHY to automatically transmit resume signaling. | RW | 0 |
Refer to USB specification 7.1.7.7 and 7.9 for more details. | ||||
0 = AutoResume disabled (default) | ||||
1 = AutoResume enabled | ||||
3 | CLOCKSUSPENDM | Active low clock suspend. Valid only in Serial Modes. Powers down the internal clock circuitry only. Valid only when SuspendM = 1b. The PHY must ignore ClockSuspend when SuspendM = 0b. By default, the clock will not be powered in Serial and Carkit Modes. | RW | 0 |
0b : Clock will not be powered in Serial and UART Modes. | ||||
1b : Clock will be powered in Serial and UART Modes. | ||||
2 | CARKITMODE | Changes the ULPI interface to UART interface. The PHY automatically clear this field when UART mode is exited. | RW | 0 |
0b: UART disabled. | ||||
1b: Enable serial UART mode. | ||||
1 | FSLSSERIALMODE_3PIN | Changes the ULPI interface to 3-pin Serial. | RW | 0 |
The PHY must automatically clear this field when serial mode is exited. | ||||
0b: FS/LS packets are sent using parallel interface | ||||
1b: FS/LS packets are sent using 3-pin serial interface | ||||
0 | FSLSSERIALMODE_6PIN | Changes the ULPI interface to 6-pin Serial. | RW | 0 |
The PHY must automatically clear this field when serial mode is exited. | ||||
0b: FS/LS packets are sent using parallel interface | ||||
1b: FS/LS packets are sent using 6-pin serial interface |
ADDRESS OFFSET | 0x08 | ||
PHYSICAL ADDRESS | 0x08 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the ifc_ctrl register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
INTERFACE_PROTECT_DISABLE | INDICATORPASSTHRU | INDICATORCOMPLEMENT | AUTORESUME | CLOCKSUSPENDM | CARKITMODE | FSLSSERIALMODE_3PIN | FSLSSERIALMODE_6PIN |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | INTERFACE_PROTECT_DISABLE | RW | 0 | |
6 | INDICATORPASSTHRU | RW | 0 | |
5 | INDICATORCOMPLEMENT | RW | 0 | |
4 | AUTORESUME | RW | 0 | |
3 | CLOCKSUSPENDM | RW | 0 | |
2 | CARKITMODE | RW | 0 | |
1 | FSLSSERIALMODE_3PIN | RW | 0 | |
0 | FSLSSERIALMODE_6PIN | R | 0 |
ADDRESS OFFSET | 0x09 | ||
PHYSICAL ADDRESS | 0x09 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the ifc_ctrl register with read/clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
INTERFACE_PROTECT_DISABLE | IN DICATORPASSTHRU | INDICATORCOMPLEMENT | AUTORESUME | CLOCKSUSPENDM | CARKITMODE | FSLSSERIALMODE_3PIN | FSLSSERIALMODE_6PIN |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | INTERFACE_PROTECT_DISABLE | RW | 0 | |
6 | INDICATORPASSTHRU | RW | 0 | |
5 | INDICATORCOMPLEMENT | RW | 0 | |
4 | AUTORESUME | RW | 0 | |
3 | CLOCKSUSPENDM | RW | 0 | |
2 | CARKITMODE | RW | 0 | |
1 | FSLSSERIALMODE_3PIN | RW | 0 | |
0 | FSLSSERIALMODE_6PIN | R | 0 |
ADDRESS OFFSET | 0x0A | ||
PHYSICAL ADDRESS | 0x0A | INSTANCE | USB_SCUSB |
DESCRIPTION | Controls UTMI+ OTG functions of the PHY. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
USEEXTERNALVBUSINDICATOR | DRVVBUSEXTERNAL | DRVVBUS | CHRGVBUS | DISCHRGVBUS | DMPULLDOWN | DPPULLDOWN | IDPULLUP |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET | |
---|---|---|---|---|---|
7 | USEEXTERNALVBUSINDICATOR | Tells the PHY to use an external VBUS over-current indicator. | RW | 0 | |
EXTERNALVBUSINDICATOR input signal is the FAULT input pin of TUSB1211. | |||||
0b: Use the internal OTG comparator (VA_VBUS_VLD) or internal VBUS valid indicator (default) | |||||
1b: Use external VBUS valid indicator signal. | |||||
6 | DRVVBUSEXTERNAL | Selects between the internal and the external 5 V VBUS supply. | RW | 0 | |
0b: Drive VBUS using the internal charge pump. | |||||
This function does nothing as TUSB1211 does not include an internal charge-pump (default) | |||||
1b: Drive VBUS using external supply (assert PSW pin). | |||||
5 | DRVVBUS | Signals the internal charge pump to drive 5 V on VBUS. | RW | 0 | |
0b : do not drive VBUS (deassert PSW pin) | |||||
1b : drive 5V on VBUS (assert PSW pin) | |||||
4 | CHRGVBUS | Charge VBUS through a resistor. Used for VBUS pulsing SRP. The Link must first check that VBUS has been discharged (see DischrgVbus register bit), and that both DP and DM data lines have been low (SE0) for 2 ms. | RW | 0 | |
0b : do not charge VBUS | |||||
1b : charge VBUS | |||||
3 | DISCHRGVBUS | Discharge VBUS through a resistor. If the Link sets this bit to 1, it waits for an RX CMD indicating SessEnd has transitioned from 0 to 1, and then resets this bit to 0 to stop the discharge. | RW | 0 | |
0b : do not discharge VBUS | |||||
1b : discharge VBUS | |||||
2 | DMPULLDOWN | Enables the 15 kΩ pulldown resistor on DM. | RW | 1 | |
0b : Pulldown resistor not connected to DM. | |||||
1b : Pulldown resistor connected to DM. | |||||
1 | DPPULLDOWN | Enables the 15 kΩ pulldown resistor on DP. | RW | 1 | |
0b : pulldown resistor not connected to DP. | |||||
1b : pulldown resistor connected to DP. | |||||
0 | IDPULLUP | Connects a pullup to the ID line and enables sampling of the signal level. | RW | 0 | |
0b : | Disable sampling of ID line. when IDPULLUP_WK_EN = 0 | ||||
Enable sampling of the ID line when IDPULLUP_WK_EN = 1 | |||||
Note Weak pull-up (RID_UP_WK) on ID is enabled when IDPULLUP = 0 to avoid floating condition, but sampling is not enabled unless IDPULLUP_WK_EN = 1 | |||||
1b : | Enable sampling of ID line and strong pullup resistor (RID_UP) on ID | ||||
Note: If ACA_DET_EN=1, then ID strong pullup resistor will be enabled automatically during ACA detection states (ACA_DETECTION, ACA_SETUP) of the charger detection state-machine , irrespective of status of IDPULLUP bit. This is to ensure correct functionality of ID ACA RA/RB/RC detection comparators. Otherwise ID pullup is controlled as described above. |
ADDRESS OFFSET | 0x0B | ||
PHYSICAL ADDRESS | 0x0B | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the otg_ctrl register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
USEEXTERNALVBUSINDICATOR | DRVVBUSEXTERNAL | DRVVBUS | CHRGVBUS | DISCHRGVBUS | DMPULLDOWN | DPPULLDOWN | IDPULLUP |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | USEEXTERNALVBUSINDICATOR | RW | 0 | |
6 | DRVVBUSEXTERNAL | RW | 0 | |
5 | DRVVBUS | RW | 0 | |
4 | CHRGVBUS | RW | 0 | |
3 | DISCHRGVBUS | RW | 0 | |
2 | DMPULLDOWN | RW | 1 | |
1 | DPPULLDOWN | RW | 1 | |
0 | IDPULLUP | RW | 0 |
ADDRESS OFFSET | 0x0C | ||
PHYSICAL ADDRESS | 0x0C | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the otg_ctrl register with read/Clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
USEEXTERNALVBUSINDICATOR | DRVVBUSEXTERNAL | DRVVBUS | CHRGVBUS | DISCHRGVBUS | DMPULLDOWN | DPPULLDOWN | IDPULLUP |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | USEEXTERNALVBUSINDICATOR | RW | 0 | |
6 | DRVVBUSEXTERNAL | RW | 0 | |
5 | DRVVBUS | RW | 0 | |
4 | CHRGVBUS | RW | 0 | |
3 | DISCHRGVBUS | RW | 0 | |
2 | DMPULLDOWN | RW | 1 | |
1 | DPPULLDOWN | RW | 1 | |
0 | IDPULLUP | RW | 0 |
ADDRESS OFFSET | 0x0D | ||
PHYSICAL ADDRESS | 0x0D | INSTANCE | USB_SCUSB |
DESCRIPTION | If set, the bits in this register cause an interrupt event notification to be generated when the corresponding PHY signal changes from low to high. By default, all transitions are enabled. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_RISE | SESSEND_RISE | SESSVALID_RISE | VBUSVALID_RISE | HOSTDISCONNECT_RISE |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_RISE | Generate an interrupt event notification when IdGnd changes from low to high. | RW | 1 |
Event is automatically masked if IdPullup bit is clear to 0 and for 50ms after IdPullup is set to 1. | ||||
3 | SESSEND_RISE | Generate an interrupt event notification when SessEnd changes from low to high. | RW | 1 |
2 | SESSVALID_RISE | Generate an interrupt event notification when SessValid changes from low to high. SessValid is the same as UTMI+ AValid. | RW | 1 |
1 | VBUSVALID_RISE | Generate an interrupt event notification when VbusValid changes from low to high. | RW | 1 |
0 | HOSTDISCONNECT_RISE | Generate an interrupt event notification when Hostdisconnect changes from low to high. Applicable only in host mode (DpPulldown and DmPulldown both set to 1b). | RW | 1 |
ADDRESS OFFSET | 0x0E | ||
PHYSICAL ADDRESS | 0x0E | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the usb_int_en_rise register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_RISE | SESSEND_RISE | SESSVALID_RISE | VBUSVALID_RISE | HOSTDISCONNECT_RISE |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_RISE | RW | 1 | |
3 | SESSEND_RISE | RW | 1 | |
2 | SESSVALID_RISE | RW | 1 | |
1 | VBUSVALID_RISE | RW | 1 | |
0 | HOSTDISCONNECT_RISE | RW | 1 |
ADDRESS OFFSET | 0x0F | ||
PHYSICAL ADDRESS | 0x0F | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the usb_int_en_rise register with read/clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_RISE | SESSEN D_RISE | SESSVALID_RISE | VBUSVALID_RISE | HOSTDISCONNECT_RISE |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_RISE | RW | 1 | |
3 | SESSEND_RISE | RW | 1 | |
2 | SESSVALID_RISE | RW | 1 | |
1 | VBUSVALID_RISE | RW | 1 | |
0 | HOSTDISCONNECT_RISE | RW | 1 |
ADDRESS OFFSET | 0x10 | ||
PHYSICAL ADDRESS | 0x10 | INSTANCE | USB_SCUSB |
DESCRIPTION | If set, the bits in this register cause an interrupt event notification to be generated when the corresponding PHY signal changes from low to high. By default, all transitions are enabled. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_FALL | SESSEND_FALL | SESSVALID_FALL | VBUSVALID_FALL | HOSTDISCONNECT_FALL |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_FALL | Generate an interrupt event notification when IdGnd changes from high to low. | RW | 1 |
Event is automatically masked if IdPullup bit is clear to 0 and for 50ms after IdPullup is set to 1. | ||||
3 | SESSEND_FALL | Generate an interrupt event notification when SessEnd changes from high to low. | RW | 1 |
2 | SESSVALID_FALL | Generate an interrupt event notification when SessValid changes from high to low. SessValid is the same as UTMI+ AValid. | RW | 1 |
1 | VBUSVALID_FALL | Generate an interrupt event notification when VbusValid changes from high to low. | RW | 1 |
0 | HOSTDISCONNECT_FALL | Generate an interrupt event notification when Hostdisconnect changes from high to low. Applicable only in host mode (DpPulldown and DmPulldown both set to 1b). | RW | 1 |
ADDRESS OFFSET | 0x11 | ||
PHYSICAL ADDRESS | 0x11 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the usb_int_en_fall register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action) |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_FALL | SESSEND_FALL | SESSVALID_FALL | VBUSVALID_FALL | HOSTDISCONNECT_FALL |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_FALL | RW | 1 | |
3 | SESSEND_FALL | RW | 1 | |
2 | SESSVALID_FALL | RW | 1 | |
1 | VBUSVALID_FALL | RW | 1 | |
0 | HOSTDISCONNECT_FALL | RW | 1 |
ADDRESS OFFSET | 0x12 | ||
PHYSICAL ADDRESS | 0x12 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the usb_int_en_fall register with read/clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_FALL | SESSEND_FALL | SESSVALID_FALL | VBUSVALID_FALL | HOSTDISCONNECT_FALL |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_FALL | RW | 1 | |
3 | SESSEN D_FALL | RW | 1 | |
2 | SESSVALID_FALL | RW | 1 | |
1 | VBUSVALID_FALL | RW | 1 | |
0 | HOSTDISCONNECT_FALL | RW | 1 |
ADDRESS OFFSET | 0x13 | ||
PHYSICAL ADDRESS | 0x13 | INSTANCE | USB_SCUSB |
DESCRIPTION | Indicates the current value of the interrupt source signal. | ||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND | SESSEND | SESSVALID | VBUSVALID | HOSTDISCONNECT |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND | Current value of UTMI+ IdGnd output. | R | 0 |
This bit is not updated if IdPullup bit is reset to 0 and for 50 ms after IdPullup is set to 1. | ||||
3 | SESSEND | Current value of UTMI+ SessEnd output. | R | 0 |
2 | SESSVALID | Current value of UTMI+ SessValid output. SessValid is the same as UTMI+ AValid. | R | 0 |
1 | VBUSVALID | Current value of UTMI+ VbusValid output. | R | 0 |
0 | HOSTDISCONNECT | Current value of UTMI+ Hostdisconnect output. | R | 0 |
Applicable only in host mode. | ||||
Automatically reset to 0 when Low Power Mode is entered. | ||||
NOTE: Reset value is '0' when host is connected. | ||||
Reset value is '1' when host is disconnected. |
ADDRESS OFFSET | 0x14 | ||
PHYSICAL ADDRESS | 0x14 | INSTANCE | USB_SCUSB |
DESCRIPTION | These bits are set by the PHY when an unmasked change occurs on the corresponding internal signal. The PHY will automatically clear all bits when the Link reads this register, or when Low Power Mode is entered. The PHY also clears this register when Serial Mode or Carkit Mode is entered regardless of the value of ClockSuspendM. The PHY follows the rules defined in Table 26 of the ULPI spec for setting any latch register bit. It is important to note that if register read data is returned to the Link in the same cycle that a USB Interrupt Latch bit is to be set, the interrupt condition is given immediately in the register read data and the Latch bit is not set. Note that it is optional for the Link to read the USB Interrupt Latch register in Synchronous Mode because the RX CMD byte already indicates the interrupt source directly |
||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | IDGND_LATCH | SESSEND_LATCH | SESSVALID_LATCH | VBUSVALID_LATCH | HOSTDISCONNECT_LATCH |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | R | 0 | |
6 | Reserved | R | 0 | |
5 | Reserved | R | 0 | |
4 | IDGND_LATCH | Set to 1 by the PHY when an unmasked event occurs on IdGnd. Cleared when this register is read. | R | 0 |
3 | SESSEND_LATCH | Set to 1 by the PHY when an unmasked event occurs on SessEnd. Cleared when this register is read. | R | 0 |
2 | SESSVALID_LATCH | Set to 1 by the PHY when an unmasked event occurs on SessValid. Cleared when this register is read. SessValid is the same as UTMI+ AValid. | R | 0 |
1 | VBUSVALID_LATCH | Set to 1 by the PHY when an unmasked event occurs on VbusValid. Cleared when this register is read. | R | 0 |
0 | HOSTDISCONNECT_LATCH | Set to 1 by the PHY when an unmasked event occurs on Hostdisconnect. Cleared when this register is read. Applicable only in host mode. | R | 0 |
NOTE: As this IT is enabled by default, the reset value depends on the host status | ||||
Reset value is '0' when host is connected. | ||||
Reset value is '1' when host is disconnected. |
ADDRESS OFFSET | 0x15 | ||
PHYSICAL ADDRESS | 0x15 | INSTANCE | USB_SCUSB |
DESCRIPTION | Indicates the current value of various signals useful for debugging. | ||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | LINESTATE |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET | |
---|---|---|---|---|---|
7 | Reserved | R | 0 | ||
6 | Reserved | R | 0 | ||
5 | Reserved | R | 0 | ||
4 | Reserved | R | 0 | ||
3 | Reserved | R | 0 | ||
2 | Reserved | R | 0 | ||
1:0 | LINESTATE | These signals reflect the current state of the single ended receivers. They directly reflect the current state of the DP (LineState[0]) and DM (LineState[1]) signals. | R | 0x0 | |
Read 0x0: | SE0 (LS/FS), Squelch (HS/Chirp) | ||||
Read 0x1: | LS: 'K' State, | ||||
FS: 'J' State, | |||||
HS: !Squelch, | |||||
Chirp: !Squelch and HS_Differential_Receiver_Output | |||||
Read 0x2: | LS: 'J' State, | ||||
FS: 'K' State, | |||||
HS: Invalid, | |||||
Chirp: !Squelch and !HS_Differential_Receiver_Output | |||||
Read 0x3: | SE1 (LS/FS), Invalid (HS/Chirp) |
ADDRESS OFFSET | 0x16 | ||
PHYSICAL ADDRESS | 0x16 | INSTANCE | USB_SCUSB |
DESCRIPTION | Empty register byte for testing purposes. Software can read, write, set, and clear this register and the PHY functionality will not be affected. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
SCRATCH |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | SCRATCH | Scratch data. | RW | 0x00 |
ADDRESS OFFSET | 0x17 | ||
PHYSICAL ADDRESS | 0x17 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the scratch_reg register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
SCRATCH |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | SCRATCH | RW | 0x00 |
ADDRESS OFFSET | 0x18 | ||
PHYSICAL ADDRESS | 0x18 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the scratch_reg with read/clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
SCRATCH |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7:0 | SCRATCH | RW | 0x00 |
ADDRESS OFFSET | 0x3D | ||
PHYSICAL ADDRESS | 0x3D | INSTANCE | USB_SCUSB |
DESCRIPTION | Power Control register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
HWDETECT | DP_VSRC_EN | VDAT_DET | DP_WKPU_EN | BVALID_FALL | BVALID_RISE | DET_COMP | SW_CONTROL |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | HWDETECT |
When SW_CONTROL= 0, HWDETECT bit is read-only. This bit indicates if the transceiver is connected to a Charging Port (Dedicated Charging Port or Charging Downstream Port ). 0b: No charger detected. 1b: Charger detected. Note when SW_CONTROL=0, hardware controls the CHRG_DET pin with the same logic described below for SW_CONTROL=1 case. When SW_CONTROL=1, HWDETECT is writeable. This bit allows manual control over the logic levels on the CHRG_DET pin. 0b: CHRG_DET is externally pulled LOW (CHRG_DET_POL is HIGH) or CHRG_DET is externally pulled HIGH (CHRG_DET_POL is LOW). 1b: CHRG_DET is driven LOW (CHRG_DET_POL is LOW) or CHRG_DET is driven HIGH (CHRG_DET_POL is HIGH) |
RW | 0 |
6 | DP_VSRC_EN |
This bit controls whether DP is allowed to send VDAT_SRC, which is a sensing voltage for charger detection. This bit also enables IDAT_SINK on DM and VDAT_REF. (Used when manual control over the charger detection is needed.) Note when SW_CONTROL=0, this bit is read-only. In this case hardware controls IDAT_SINK and VDAT_REF with the same logic described below for SW_CONTROL=1 case. When SW_CONTROL=1, DP_VSRC_EN is writeable: 0b: No transmission of sensing voltage is performed. IDAT_SINK and VDAT_REF are disabled. 1b: DP transmits sensing voltage; enables IDAT_SINK and VDAT_REF. |
RW | 0 |
5 | VDAT_DET |
This bit indicates the presence of a voltage level higher that VDAT_REF on the DM. (Used when manual control over the charger detection is needed.) 0b: Voltage on DM is lower than VDAT_REF 1b: Voltage on DM is higher than VDAT_REF |
RW | 0 |
4 | DP_WKPU_EN |
Enables the weak pull-up resistor on the DP pin in synchronous mode when VBUS is above the VSESS_VLD threshold. 0b: DP weak pull-up is disabled. 1b: DP weak pull-up is enabled when VBUS > VSESS_VLD Detection of DP/DM condition while this bit is set should be done through LINESTATE<1:0>bits in DEBUG register (0x15) or through RX CMD. |
RW | 0 |
3 | BVALID_FALL | Enables RX CMD’s for high to low transitions on BVALID. When BVALID changes from high to low, the USB TRANS will send an RX CMD to the link with the alt_int bit set to 1b. This bit is optional and is not necessary for OTG devices. This bit is provided for debugging purposes. Disabled by default. | RW | 0 |
2 | BVALID_RISE | Enables RX CMD’s for low to high transitions on BVALID. When BVALID changes from low to high, the USB Trans will send an RX CMD to the link with the alt_int bit set to 1b. This bit is optional and is not necessary for OTG devices. This bit is provided for debugging purposes. Disabled by default. | RW | 0 |
1 | DET_COMP |
This bit indicates if a Charging Port has been detected. 0b: A Charging Port has not been detected, or charger detection has not been activated. (Identical to HWDETECT) 1b: A Charging Port has been detected (Identical to HWDETECT) When SW_CONTROL = 1 this bit is reset to 0. |
RW | 0 |
0 | SW_CONTROL |
This bit controls whether CHRG_DET pin is controlled automatically or manually. When manual control is required, the software must set the SW_CONTROL bit to logic 1 in the first register access, followed by issuing a second register access to set or clear the HWDETECT bit. Software must never set the SW_CONTROL bit and change the HWDETECT bit in the same register access. 0b: The CHRG_DET pin will be asserted or deasserted depending on the automatic USB charger detection result. 1b: At rising-edge of SW_CONTROL bit save current hardware charger detection context and hand-off control to software:
Therefore if charger detection has been initiated in dead-battery condition (while the chip is disabled (CS=0)), VDP_SRC will remain enabled and CHRG_DET pin status will not change when SW takes control, and SW can read register status before deciding to perform further charger/device/accessory detection or USB attach The CHRG_DET pin will be asserted or deasserted depending on the HWDETECT bit setting. |
RW | 0 |
ADDRESS OFFSET | 0x3E | ||
PHYSICAL ADDRESS | 0x3E | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the POWER_CONTROL register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
HWDETECT | DP_VSRC_EN | VDAT_DET | DP_WKPU_EN | BVALID_FALL | BVALID_RISE | DET_COMP | SW_CONTROL |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | HWDETECT | RW | 0 | |
6 | DP_VSRC_EN | RW | 0 | |
5 | VDAT_DET | R | 0 | |
4 | DP_WKPU_EN | RW | 0 | |
3 | BVALID_FALL | RW | 0 | |
2 | BVALID_RISE | RW | 0 | |
1 | DET_COMP | R | 0 | |
0 | SW_CONTROL | RW | 0 |
ADDRESS OFFSET | 0x3F | ||
PHYSICAL ADDRESS | 0x3F | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the POWER_CONTROL register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
HWDETECT | DP_VSRC_EN | VDAT_DET | DP_WKPU_EN | BVALID_FALL | BVALID_RISE | DET_COMP | SW_CONTROL |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | HWDETECT | RW | 0 | |
6 | DP_VSRC_EN | RW | 0 | |
5 | VDAT_DET | R | 0 | |
4 | DP_WKPU_EN | RW | 0 | |
3 | BVALID_FALL | RW | 0 | |
2 | BVALID_RISE | RW | 0 | |
1 | DET_COMP | R | 0 | |
0 | SW_CONTROL | RW | 0 |
ADDRESS OFFSET | 0x80 | ||
PHYSICAL ADDRESS | 0x80 | INSTANCE | USB_SCUSB |
DESCRIPTION | Eye diagram programmability and DP/DM swap control | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | DATAPOLARITY | ZHSDRV | IHSTX |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | DATAPOLARITY |
Control data polarity on DP/DM DATAPOLARITY bit will control both DP/DM polarity in USB PHY and Charger Detection polarity in active mode but not charger detection in polarity in dead battery condition. 0b: DP & DM polarity is swapped DP is mapped to C1 pin, DM mapped to D1 pin 1b: DP & DM polarity is not swapped DP is mapped to D1 pin, DM mapped to C1 pin as described in Terminal description chapter |
RW | 1 |
5:4 | ZHSDRV |
High speed output impedance configuration for eye diagram tuning : 00 45.455 Ω 01 43.779 Ω 10 42.793 Ω 11 42.411 Ω |
RW | 0x0 |
3:0 | IHSTX |
High speed output drive strength configuration for eye diagram tuning :
0000 17.928 mA 0001 18.117 mA 0010 18.306 mA 0011 18.495 mA 0100 18.683 mA 0101 18.872 mA 0110 19.061 mA 0111 19.249 mA 1000 19.438 mA 1001 19.627 mA 1010 19.816 mA 1011 20.004 mA 1100 20.193 mA 1101 20.382 mA 1110 20.570 mA 1111 20.759 mA IHSTX[0] is also the AC BOOST enable IHSTX[0] = 0 → AC BOOST is disabled IHSTX[0] = 1 → AC BOOST is enabled |
RW | 0x1 |
ADDRESS OFFSET | 0x81 | ||
PHYSICAL ADDRESS | 0x81 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as VENDOR_SPECIFIC1 register with read/set-only property (write '1' to set a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATEN CY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | DATAPOLARITY | ZHSDRV | IHSTX |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | DATAPOLARITY | RW | 1 | |
5:4 | ZHSDRV | RW | 0x0 | |
3:0 | IHSTX | RW | 0x1 |
ADDRESS OFFSET | 0x82 | ||
PHYSICAL ADDRESS | 0x82 | INSTANCE | USB_SCUSB |
DESCRIPTION | This register doesn't physically exist. It is the same as the VENDOR_SPECIFIC1 register with read/clear-only property (write '1' to clear a particular bit, a write '0' has no-action). |
||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | DATAPOLARITY | ZHSDRV | IHSTX |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | DATAPOLARITY | RW | 1 | |
5:4 | ZHSDRV | RW | 0x0 | |
3:0 | IHSTX | RW | 0x1 |
ADDRESS OFFSET | 0x83 | ||
PHYSICAL ADDRESS | 0x83 | INSTANCE | USB_SCUSB |
DESCRIPTION | Indicates the current value of the interrupt source signal. | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
VBUS_MNTR_STS | REG3V3IN_MNTR_STS | SVLDCONWKB_WDOG_STS | ID_FLOAT_STS | ID_RARBRC_STS<1:0> | Reserved | BVALID_STS |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | VBUS_MNTR_STS | Current value of VBUS_MNTR comparator | R | 0 |
6 | REG3V3IN_MNTR_STS |
Current value of REG3V3IN_MNTR comparator 0: VBAT REG3V3IN_MNTR threshold 1: VBAT REG3V3IN_MNTR threshold |
R | 0 |
5 | SVLDCONWKB_WDOG_STS | Current value of SVLDCONWKB_WDOG status. | R | 0 |
0: Watchdog timer has not expired | ||||
1: Watchdog timer has expired | ||||
4 | ID_FLOAT_STS | Current value of ID_FLOAT detection on ID pin | R | 0 |
0: If RID_FLOAT not detected | ||||
1: If RID_FLOAT detected | ||||
3:2 | ID_RARBRC_STS<1:0> |
ACA Detection status output 00: ACA not detected 01: R_ID_A resistance on ID detected 10: R_ID_B resistance on ID detected 11: R_ID_C resistance on ID detected |
R | 0x0 |
1 | Reserved | R | 0 | |
0 | BVALID_STS | Current value of VB_SESS_VLD output | R | 0 |
ADDRESS OFFSET | 0x84 | ||
PHYSICAL ADDRESS | 0x84 | INSTANCE | USB_SCUSB |
DESCRIPTION | These bits are set by the PHY when an unmasked change occurs on the corresponding internal signal. The PHY will automatically clear all bits when the Link reads this register, or when Low Power Mode is entered. The PHY also clears this register when Serial mode is entered regardless of the value of ClockSuspendM. The PHY follows the rules defined in Table 26 of the ULPI spec for setting any latch register bit. |
||
TYPE | R | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
VBUS_MNTR_LATCH | REG3V3IN_MNTR_LATCH | SVLDCONWKB_WDOG _LATCH | ID_FLOAT_LATCH | ID_RARBRC_LATCH<1:0> | Reserved | BVALID_LATCH |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | VBUS_MNTR_LATCH | Set to ‘1’ when an unmasked event occurs on VBUS_MNTR comparator Clear on read register. | R | 0 |
6 | REG3V3IN_MNTR_LATCH | Set to ‘1’ when an unmasked event occurs on REG3V3IN_MNTR. comparator Clear on read register. | R | 0 |
5 | SVLDCONWKB_WDOG _LATCH | Set to ‘1’ when an unmasked event occurs on SVLDCONWKB_WDOG,that is,, when watchdog counter has expired. Clear on read register. | R | 0 |
4 | ID_FLOAT_LATCH | Set to ‘1’ when an unmasked event occurs on ID_FLOAT detection. Clear on read register. | R | 0 |
3:2 | ID_RARBRC_LATCH<1:0> |
Set according to table below when an unmasked event occurs on ACA Detection status output 00: No ACA event detected 01: ACA event. Detected 10: ACA event. Detected 11: ACA event. Detected |
R | 0x0 |
1 | Reserved | R | 0 | |
0 | BVALID_LATCH | Set to ‘1’ when an unmasked event occurs on VB_SESS_VLD comparator. Clear on read register. | R | 0 |
ADDRESS OFFSET | 0x85 | ||
PHYSICAL ADDRESS | 0x85 | INSTANCE | USB_SCUSB |
DESCRIPTION | |||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | CHGD_IDP_SRC_EN _EN | IDPULLUP_WK_EN | SW_USB_DET | DATA_CONTACT_DET_EN | REG3V3_VSEL<2:0> |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | Software must not set this bit | RW | 0 |
6 | CHGD_IDP_SRC_EN | Enable IDP_SRC on DP and RDM_DWN on DM.Can be used to perform data contact detect (Used when manual control over the charger detection is needed.) When SW_CONTROL=0 this bit is Read-only and gives the status of IDP_SRC control signal in charger detection FSM. When SW_CONTROL=1, this bit is Read/Write: | RW | 0 |
0b: IDP_SRC on DP and RDM_DWN on DM are disabled. | ||||
1b: IDP_SRC on DP and RDM_DWN on DM are enabled | ||||
Note: Conflict resolution case: If DP_VSRC_EN = 1 at the same time as this bit is set, then IDP_SRC on DP and RDM_DWN on DM are disabled, (and VDPSRC will remain enabled). | ||||
5 | IDPULLUP_WK_EN | Enable of sampling of ID line with RID_WK_PU. This bit is ignored when IDPULLUP = 1 Refer to IDPULLUP bit description | RW | 0 |
0b: Disable sampling of ID line | ||||
1b: Enable sampling of the ID line with custom RID_UP_WK | ||||
4 | SW_USB_DET | Battery Charger Detection state-machine enable bit | RW | 0 |
0b: Disable Battery Charger Detection State machine | ||||
1b: Enable Battery Charger Detection State-machine if SW_CONTROL = 0 | ||||
Note: This bit is automatically set to 1 by hardware during Dead Battery Detection. When the chip is powered up and enters ACTIVE mode this bit can be read to check if Charger Detection FSM is active. Setting this bit to 0 will stop Battery Charger Detection that was initiated during Dead Battery Condition. This bit is reset automatically when SW_CONTROL bit is 1. This bit is reset to 0 by RESETN pin This bit will also be reset to 0 if SVLDCONWKB_CNTR timeout occurs. Software must then write this bit to 1 to reenable Battery Charger Detection state-machine if required. | ||||
3 | DATA_CONTACT_DET_EN | If state-machine is enabled in active mode (through SW_USB_DET bit above) and this bit is set to 1, then Data Contact Detection will be enabled in the charger detection state-machine. This optional feature is disabled by default. | RW | 0 |
2:0 | REG3V3_VSEL<2:0> | When 000 REG3V3 = 2.5 V | RW | 0x3 |
When 001 REG3V3 = 2.75 V | ||||
When 010 REG3V3 = 3.0 V | ||||
When 011 REG3V3 = 3.10 V (default) | ||||
When 100 REG3V3 = 3.20 V | ||||
When 101 REG3V3 = 3.30 V | ||||
When 110 REG3V3 = 3.40 V | ||||
When 111 REG3V3 = 3.50 V |
ADDRESS OFFSET | 0x86 | ||
PHYSICAL ADDRESS | 0x86 | INSTANCE | USB_SCUSB |
DESCRIPTION | |||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | CHGD_IDP_SRC_EN | IDPULLUP_WK_EN | SW_USB_DET | DATA_CONTACT_DET_EN | REG3V3_VSEL<2:0> |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | CHGD_IDP_SRC_EN | RW | 0 | |
5 | IDPULLUP_WK_EN | RW | 0 | |
4 | SW_USB_DET | RW | 0 | |
3 | DATA_CONTACT_DET_EN | RW | 0 | |
2:0 | REG3V3_VSEL<2:0> | RW | 0x3 |
ADDRESS OFFSET | 0x87 | ||
PHYSICAL ADDRESS | 0x87 | INSTANCE | USB_SCUSB |
DESCRIPTION | |||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | CHGD_IDP_SRC_EN | IDPULLUP_WK_EN | SW_USB_DET | DATA_CONTACT_DET_EN | REG3V3_VSEL<2:0> |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | CHGD_IDP_SRC_EN | RW | 0 | |
5 | IDPULLUP_WK_EN | RW | 0 | |
4 | SW_USB_DET | RW | 0 | |
3 | DATA_CONTACT_DET_EN | RW | 0 | |
2:0 | REG3V3_VSEL<2:0> | RW | 0x3 |
ADDRESS OFFSET | 0x88 | ||
PHYSICAL ADDRESS | 0x88 | INSTANCE | USB_SCUSB |
DESCRIPTION | Charger Detection SERX Status and PSW,VBUS ext resistor configuration register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | ACA_DET_EN | RABUSIN_EN | R1KSERIES | PSW_OSOD | PSW_CMOS | CHGD_SERX_DP | CHGD_SERX_DM |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | ACA_DET_EN | This bit is used to enable Accessory Charger Adapter (ACA) detection in Battery Charger State-Machine in active-mode | RW | 1 |
5 | RABUSIN_EN |
This bit is used modify VBUS resistance to ground. 0: A-Device VBUS resistor RVBUS_IDLE_A is disabled. VBUS resistance to ground becomes RVBUS_IDLE_B (see Section 4.18) 1: A-Device VBUS resistor RVBUS_IDLE_A is enabled (see Section 4.18) |
RW | 1 |
4 | R1KSERIES |
This bit is used to indicate to TUSB1211 whether an external series 1kohm resistor is connected on VBUS. When this bit is set internal VBUS comparator thresholds are adjusted so they remain in spec. 0: No external series resistor on VBUS 1: An external 1=kΩ series resistor is connected on VBUS |
RW | 1 |
3 | PSW_OSOD |
This bit controls PSW pin configuration. It can be overridden by PSW_CMOS bit below ‘0’: PSW pad is in OS mode (active high) ‘1’: PSW pad is in OD mode (active low) |
RW | 0 |
2 | PSW_CMOS |
This bit controls PSW pin configuration. It overrides PSW_OSOD bit above. ‘0’ : PSW pad is in OD or OS mode (controlled by PSW_OD bit) ‘1’: PSW pad is in CMOS mode |
RW | 0x0 |
1 | CHGD_SERX_DP |
Read-only status bit showing status of debounced charger detection single-ended receiver comparator on DP 0: VDP < [0.8V : 2.0V] SERX threshold 1: VDP > [0.8V : 2.0V] SERX threshold Note: This comparator and status bit is enabled automatically in the following scenarios:
In all other cases (including when DP 1.5K pullup is enabled by SW for CDP/DCP/SDP differentiation after SW charger detection step) this status bit should be ignored and LINESTATE<1:0> bits in DEBUG register, or RXCMD should be used for DP/DM detection |
R | 0x0 |
0 | CHGD_SERX_DM |
Read-only status bit showing status of debounced charger detection single-ended receiver comparator on DM 0: VDM < [0.8V : 2.0V] SERX threshold 1: VDM > [0.8V : 2.0V] SERX threshold Note: This comparator and status bit is enabled automatically in the following scenarios:
In all other cases (including when DP 1.5K pullup is enabled by SW for CDP/DCP/SDP differentiation after SW charger detection step) this status bit should be ignored and LINESTATE<1:0> bits in DEBUG register, or RXCMD should be used for DP/DM detection |
R | 0x0 |
ADDRESS OFFSET | 0x89 | ||
PHYSICAL ADDRESS | 0x89 | INSTANCE | USB_SCUSB |
DESCRIPTION | Charger Detection SERX Status and PSW,VBUS ext resistor configuration register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | ACA_DET_EN | RABUSIN_EN | R1KSERIES | PSW_OSOD | PSW_CMOS | CHGD_SERX_DP | CHGD_SERX_DM |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | ACA_DET_EN | RW | 1 | |
5 | RABUSIN_EN | RW | 1 | |
4 | R1KSERIES | RW | 1 | |
3 | PSW_OSOD | RW | 0 | |
2 | PSW_CMOS | RW | 0x0 | |
1 | CHGD_SERX_DP | R | 0x0 | |
0 | CHGD_SERX_DM | R | 0x0 |
ADDRESS OFFSET | 0x8A | ||
PHYSICAL ADDRESS | 0x8A | INSTANCE | USB_SCUSB |
DESCRIPTION | Charger Detection SERX Status and PSW,VBUS ext resistor configuration register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | ACA_DET_EN | RABUSIN_EN | R1KSERIES | PSW_OSOD | PSW_CMOS | CHGD_SERX_DP | CHGD_SERX_DM |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | ACA_DET_EN | RW | 1 | |
5 | RABUSIN_EN | RW | 1 | |
4 | R1KSERIES | RW | 1 | |
3 | PSW_OSOD | RW | 0 | |
2 | PSW_CMOS | RW | 0x0 | |
1 | CHGD_SERX_DP | R | 0x0 | |
0 | CHGD_SERX_DM | R | 0x0 |
ADDRESS OFFSET | 0x8B | ||
PHYSICAL ADDRESS | 0x8B | INSTANCE | USB_SCUSB |
DESCRIPTION | Vendor-specific interrupt enable register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | AUTORESUME_WDOG_EN | ID_FLOAT_EN | ID_RES_EN | SVLDCONWKB_WDOG _EN | VBUS_MNTR_RISE_EN | VBUS_MNTR_FALL_EN | REG3V3IN_MNTR_EN |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | AUTORESUME_WDOG_EN |
Autoresume watchdog timer enable bit 0b: Disable the Autoresume watchdog timer 1b: Enable the Autoresume watchdog timer Timer is be initialized and starts counting when the PHY detects a resume-K. |
RW | 1 |
5 | ID_FLOAT_EN | When set to ‘1’, it enables RX CMD’s for high to low or low to high transitions on ID_FLOAT. | RW | 0 |
4 | ID_RES_EN |
When set to ‘1’, this bit enables RX CMD’s for high to low or low to high transitions on detection of ACA resistors RID_A , RID_B or RID_C . When this bit is set to ‘1’ and any of the above ACA resistors are detected, TUSB1211 will send an RX CMD to the link with the alt_int bit set to 1b. The status of ACA detection can then be read back through status bits ID_RARBRC_STS <1:0> Setting this bit also forces ID pull-up (RID_UP) to be enabled irrespective of IDPULLUP bit setting |
RW | 0 |
3 | SVLDCONWKB_WDOG _EN | Generate an interrupt event notification when SVLDCONWKB_WDOG watchdog timer times out Note SVLDCONWKB_WDOG watchdog timer is enabled and disabled separately, see Section 5.3.12 for more details. | RW | 0 |
2 | VBUS_MNTR_RISE_EN | Generate an interrupt event notification when VBUS_MNTR changes from low to high. | RW | 0 |
1 | VBUS_MNTR_FALL_EN | Generate an interrupt event notification when VBUS_MNTR changes from high to low. | R | 0 |
0 | REG3V3IN_MNTR_EN |
Optional feature which can be used to indicate to Link if VBAT level is high enough to guarantee USB functionality 0b: Disable this monitoring featue 1b: Enable monitoring of REG3V3IN (=VBAT) level through RXCMD on detection of high to low or low to high transitions on comparator REG3V3IN_MNTR after debounce. |
R | 0 |
ADDRESS OFFSET | 0x8C | ||
PHYSICAL ADDRESS | 0x8C | INSTANCE | USB_SCUSB |
DESCRIPTION | Vendor-specific interrupt set register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | AUTORESUME_WDOG_EN | ID_FLOAT_EN | ID_RES_EN | SVLDCONWKB_WDOG _EN | VBUS_MNTR_RISE_EN | VBUS_MNTR_FALL_EN | REG3V3IN_MNTR_EN |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | AUTORESUME_WDOG_EN | RW | 1 | |
5 | ID_FLOAT_EN | RW | 0 | |
4 | ID_RES_EN | RW | 0 | |
3 | SVLDCONWKB_WDOG _EN | RW | 0 | |
2 | VBUS_MNTR_RISE_EN | RW | 0 | |
1 | VBUS_MNTR_FALL_EN | RW | 0 | |
0 | REG3V3IN_MNTR_EN | RW | 0 |
ADDRESS OFFSET | 0x8D | ||
PHYSICAL ADDRESS | 0x8D | INSTANCE | USB_SCUSB |
DESCRIPTION | Vendor-specific interrupt clear register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
Reserved | AUTORESUME_WDOG_EN | ID_FLOAT_EN | ID_RES_EN | SVLDCONWKB_WDOG _EN | VBUS_MNTR_RISE_EN | VBUS_MNTR_FALL_EN | REG3V3IN_MNTR_EN |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | Reserved | RW | 0 | |
6 | AUTORESUME_WDOG_EN | RW | 1 | |
5 | ID_FLOAT_EN | RW | 0 | |
4 | ID_RES_EN | RW | 0 | |
3 | SVLDCONWKB_WDOG _EN | RW | 0 | |
2 | VBUS_MNTR_RISE_EN | RW | 0 | |
1 | VBUS_MNTR_FALL_EN | RW | 0 | |
0 | REG3V3IN_MNTR_EN | RW | 0 |
ADDRESS OFFSET | 0x8E | ||
PHYSICAL ADDRESS | 0x8E | INSTANCE | USB_SCUSB |
DESCRIPTION | SOF and ACA CFG Register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
ACA_RID_B_CFG | ACA_RID_A_CFG | SOF_EN | Reserved |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | ACA_RID_B_CFG |
This bit is used to enable correct configuration of TUSB1211 as a B-device with ACA connected and nothing (or A-device OFF) at ACA Accessory port and charger present on ACA Charger Port, if ACA RID_B is detected on ID pin. It impacts: a) VA_VBUS_VLD in RX CMD b) VSESS_VLD in RX CMD c) VBUS SRP When this bit is‘1’ and RID_B is detected on ID pin , then mask VBUS plug detection information from being sent to the link, and mask OTG VBUS SRP commands (CHRGVBUS, DISCHRGVBUS bits) from the link. Set VA_VBUS_VLD =0 and VSESS_VLD =0 in RX CMD, and disable RB_SRP_UP, RB_SRP_DWN Note: CHRGVBUS, DISCHRGVBUS register bit settings themselves are unchanged but VBUS SRP pullup and pulldown are disabled. When this bit is ‘0’ RID_B detection has no impact on VA_VBUS_VLD detection and VA_SESS_VLD detection in RX CMD |
RW | 0 |
6 | ACA_RID_A_CFG |
This bit is used to enable correct configuration of TUSB1211 as an A-device with ACA connected and B-device at ACA Accessory port and charger connected to Charger Port , if ACA RID_A is detected on ID pin. It impacts: a) IDGND detection in RXCMD and b) Enabling of external VBUS on PSW pin When this bit is ‘1’ and RID_A is detected on ID pin then TUSB1211 will be configured as an A-device by set ID=0 in RXCMD (equivalent to IDGND detected). In addition PSW pin is deasserted to avoid contention on VBUS pin since the charger at ACA port already provides VBUS. When this bit is ‘0’ RID_A detection has no impact on RXCMD nor PSW pin |
RW | 0 |
5 | SOF_EN |
USB HS Start-of-Frame clock output feature enable 0: Disable HS SOF clock 1: Enable HS SOF clock output on SOF pin HS USB SOF packet rate is 8kHz |
RW | 0 |
4:0 | Reserved | RW | 0 |
ADDRESS OFFSET | 0x8F | ||
PHYSICAL ADDRESS | 0x8F | INSTANCE | USB_SCUSB |
DESCRIPTION | SOF and ACA CFG Register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
ACA_RID_B_CFG | ACA_RID_A_CFG | SOF_EN | Reserved |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | ACA_RID_B_CFG | RW | 0 | |
6 | ACA_RID_A_CFG | RW | 0 | |
5 | SOF_EN | RW | 0 | |
4:0 | Reserved | RW | 0 |
ADDRESS OFFSET | 0x90 | ||
PHYSICAL ADDRESS | 0x90 | INSTANCE | USB_SCUSB |
DESCRIPTION | SOF and ACA CFG Register | ||
TYPE | RW | ||
WRITE LATENCY |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|
ACA_RID_B_CFG | ACA_RID_A_CFG | SOF_EN | Reserved |
BITS | FIELD NAME | DESCRIPTION | TYPE | RESET |
---|---|---|---|---|
7 | ACA_RID_B_CFG | RW | 0 | |
6 | ACA_RID_A_CFG | RW | 0 | |
5 | SOF_EN | RW | 0 | |
4:0 | Reserved | RW | 0 |