JAJSQ81F December 2015 – December 2023 TUSB542
PRODUCTION DATA
Figure 7-2 shows an example implementation of an USB Type-C DRP port using TUSB542. Texas Instruments TUSB322 is shown here as channel configuration (CC) controller. Note: connections for CNFG pins of TUSB542 is an example only. The connection of the CNFG pins is application dependent; refer to the Table 6-2, where the user can find the available settings.
It is recommended to run an overall system signal integrity analysis, to estimate the channel loss and configure the re-driver. It is also recommended to have pull-up and pull-down option on the configuration pins for debug and testing purposes.
The signal integrity analysis must determine the following:
The equalization must be set based on the insertion loss in the pre-channel (channel before the TUSB542 device). The input voltage to the device is able to have a large range because of the receiver sensitivity and the available EQ settings.
The de-emphasis setting must be set based on the length and characteristics of the post channel (channel after the TUSB542 device).
The output swing setting can also be configured based on the amplitude needed to pass the compliance test. This setting is also based on the length of interconnect or cable the TUSB542 is driving.
Refer to the Table 6-2 for a detailed description on how to configure the CONFIG_A1/A2 and CONFIG_B1/A2 terminals, to achieve the desired EQ, OS, and DE settings.