JAJSEZ0B August 2014 – January 2024 UCC27511A-Q1
PRODUCTION DATA
PIN | I/O | FUNCTION | |
---|---|---|---|
NO. | NAME | ||
1 | VDD | I | Bias supply input. |
2 | OUTH | O | Sourcing current output of driver. Connet a resistor between the OUTH pin and the gate of the power- switching device to adjust turnon speed. |
3 | OUTL | O | Sinking current output of driver. Connect a resistor between the OUTL pin and the gate of the power- switching device to adjust turnoff speed. |
4 | GND | — | Ground. All signals referenced to this pin. |
5 | IN– | I | Inverting input. When the driver is used in non-inverting configuration, connect the IN– pin to GND in order to enable output. The OUTx pin is held low if the IN– pin is unbiased or floating. |
6 | IN+ | I | Non-inverting input. When the driver is used in inverting configuration, connect the IN+ pin to VDD in order to enable output. The OUTx pin is held low if the IN+ pin is unbiased or floating. |