JAJSVF6C December 2013 – September 2024 UCC27532-Q1
PRODUCTION DATA
In the inverter circuit shown in Figure 8-5, the UCC27532-Q1 drivers for the IGBTs will require the drivers to be supplied by individually isolated power supplies to enable them to drive the floating IGBT devices in the power stage.
In addition the gate drive signals from the micro-controller to the UCC27532-Q1 will also must level shifted through isolation devices.