JAJSKM1C october 2019 – september 2021 UCC5870-Q1
PRODUCTION DATA
The overall operation mode transition diagram is presented in Figure 7-37. The current state of the device is read in the STATUS1[OPM] bits (STATUS1). Note that these bits are only readable in the Configuration 2 and Active states.