JAJSKM1C october 2019 – september 2021 UCC5870-Q1
PRODUCTION DATA
The Address-based configuration provides significant flexibility to the system design. This configuration is similar to the Independent Slave configuration in that all of the CLK, SDO, and SDI connections are shared between all devices (shown in Figure 7-42). Additionally, the nCS input is also shared. This reduces the GPIO requirement on the MCU to one, similar to Daisy Chain, but also allows random access like the Independent Slave configuration. The Address-based configuration is done by defining each device in the system with a unique address. See the Device Addressing section for details on how to address the devices in the system. The message frame is shown in Figure 7-39