JAJSK73J March 2012 – November 2021 UCD3138
PRODUCTION DATA
The UCD3138 filter is a PID filter with many enhancements for power supply control. Some of its features include:
Here is the first section of the Filter :
The filter input, Xn, generally comes from a front end. Then there are three branches, P, I. and D. Note that the D branch also has a pole, Kd Alpha. Clamps are provided both on the I branch and on the D alpha pole.
The filter also supports a nonlinear mode, where up to 7 different sets of coefficients can be selected depending on the magnitude of the error input Xn. This can be used to increase the filter gain for higher errors to improve transient response.
Here is the output section of the filter (S0.23 means that there is 1 sign bit, 0 integer bits and 23 fractional bits):
This section combines the P, I, and D sections, and provides for saturation, scaling, and clamping.
There is a final section for the filter, which permits its output to be matched to the DPWM:
This permits the filter output to be multiplied by a variety of correction factors to match the DPWM Period, to provide for Voltage Feed Forward, or for other purposes. After this, there is another clamp. For resonant mode, the filter can be used to generate both period and duty cycle.