JAJSK73J March 2012 – November 2021 UCD3138
PRODUCTION DATA
At the core of the UCD3138 controller are three DDPs. Each DPP can be configured to drive from one to eight DPWM outputs. Each DPP consists of:
These can be connected in many different combinations, with multiple filters and DPWMs. They are capable of supporting functions like input voltage feed forward, current mode control, and constant current/constant power, and so forth. The simplest configuration is shown in the following figure: