JAJSHD5D November 2010 – April 2019 UCD90160
PRODUCTION DATA.
Fusion GUI can be used to design the device configuration online or offline (with or without a UCD90160 device connected to the computer). In offline mode, Fusion GUI will prompt user to create or open a project file (.xml) at launch. In online mode, Fusion GUI will automatically detect the device on PMBus and read the configuration data from the device. An USB-to-GPIO Adapter EVM (HPA172) from Texas Instruments is required to connect Fusion GUI to PMBus.
The general design steps include the following:
Details of the steps are self-explanatory in Fusion GUI.
After configuration changes, click the Write to Hardware button to apply the changes. In online mode, then click the Store RAM to Flash button to permanently store the new configuration into the device data flash.