JAJSHD6B August 2016 – May 2019 UCD90320
PRODUCTION DATA.
The UCD90320 device has an integrated power-on reset (POR) circuit which monitors the supply voltage. At power up, the POR detects the V33D pin voltage rise. When the V33D voltage is greater than VRESET, the device comes out of reset.
The device can be forced into the reset state by an external circuit connected to the RESET̅ pin. A logic-low voltage on this pin for longer than tRESET sets the device into reset state. The device comes out of reset within tIRT after RESET̅ is released to logic-high level.
Any time the device comes out of reset, it begins an initialization routine that lasts typically 40 ms. A data flash checksum verification is performed at power up. If the checksum verification does not match, the device configuration settings are cleared , the PMBALERT pin is asserted, and a flag is set in the status register. A fault-log checksum verification in the EEPROM is also performed at power up. Each log entry includes the checksum verification status. Only a corrupted log entry is discarded. During the initialization routine, all I/O pins are held at high impedance state. At the end of initialization, the device begins normal operation as defined by the device configuration.