DLPU078A july 2019 – may 2023 DLP230NP , DLPC3436
This command specifies the amount of time that must pass before edges of the INT_SUBFRAME signal, which are allowed to toggle. This function suppresses an edge that occurs too close to the previous edge. The input parameters are applied separately to the axes defined by AWG_12 and AWG_34.