DLPU114A August 2024 – November 2024 DLPC8445
The Main Application contained in the embedded software will be reached during the initialization process once the boot process is completed normally and STAY_IN_BOOT is set to 0. This mode is the primary use case for the DLP® system being the mode in which images are projected.