DLPU114A August 2024 – November 2024 DLPC8445
This command erases the sector of the flash of the given address. This command is a flash update command and requires flash operations to be unlocked using Unlock Flash for Update command. The sector address shall be specified as an offset from flash start address. For example, in a flash device where all sectors are 64KB of size, sector addresses shall be specified as follows:
Sector 0 = 0
Sector 1 = 0x10000
Sector 2 = 0x20000
...