DLPU114A August 2024 – November 2024 DLPC8445
This command is used to switch between BootROM to Application and vice versa. When a hard reset to the Boot Application is issued and pin TSTPT_0 is held high, the controller will transfer to BootROM. TSTPT_0 will only be sampled for 1us after reset or power on. If TSTPT_0 is low when the command is issued, the controller will transfer to the secondary boot.
WARNING: If command is issued for jumping to Boot Application from Main Application, then returning back to Main Application is not possible without re-programming the Main Application.