DLPU114A August 2024 – November 2024 DLPC8445
This command specifies the orientation of the image displayed on the DMD.
The command rotates and/or flips the image displayed on the DMD. Rotation can be useful for a portrait source image such as inside a mobile phone. Flips are provided to support ceiling mount and rear projection use cases.
Landscape images typically should not be rotated, but the controller allows this as it may be appropriate for some situations or configurations.
Image rotation is allowed while keystone correction or warping is enabled, though it may not be appropriate for all situations or configurations.
The user is responsible for determining if the resulting image from these commands is acceptable.
User can use the Display Size command to centre the image.
This command must be followed with a Write Execute Display command to be applied.
The following figure shows the long axis flip.
The following figure shows the short axis flip.