DLPU114A August 2024 – November 2024 DLPC8445
This command specifies the active image resolution to be output on the display module, specifies the size of the non-keystone corrected, non-warped image to be output from the scalar function. This is the resolution of the rectangular or square displayed image. The controller will determine the amount of scaling needed in x and in y based on the size of the input image. For a source image from the external video port, the controller will measure the size of the source image based on the DATEN signal. However, if the image is cropped by command Set Image Crop, the controller will use this smaller size to be scaled to fill the DMD.
The parameter values are to be 1-based such that a value of 1280 pixels displays 1280 pixels per line.
If keystone correction or warping is enabled, the resulting non-rectangular images on the DMD will all fit within the active display region specified by command Set Display Size.
If the display size exceeds the resolution available on the DMD, this is considered an error and the command does not execute. The display size parameters are checked against the DMD available resolution in both rotation image orientations (non-rotated and rotated), and if the DMD resolution is exceeded in either of these orientations, it is considered an error. The system does not check for proper image orientation setup.
If the source, crop, and display parameter combinations exceed the capabilities of the scalar, the system implements the user request as best it can, and the displayed image may be broken. The user must provide updated parameters to fix the image.
This command must be followed with a Write Execute Display command to be applied.