DLPU114A August 2024 – November 2024 DLPC8445
This command sets the input polarity detection mode for VSync and HSync signals for all external sources. The controller requires Sync signals to have active high polarity. The software can auto-detect and correct the polarity. The user should choose Automatic Mode to use this feature. Automatic Mode is the default mode. Otherwise, user can choose manual mode and provide the input polarities. The provided input polarities take effect only in manual mode. It will be used by hardware to correct the polarities.