JAJSCF6G July 2016 – December 2019 TPS2660
PRODUCTION DATA.
When the active current limiting mode is selected, during overload events, the device continuously regulates the load current to the overcurrent limit I(OL) programmed by the R(ILIM) resistor as shown in Equation 3.
where
During an overload condition, the internal current-limit amplifier regulates the output current to I(LIM). The FLT signal assert after a delay of 875 µs.The output voltage droops during the current regulation, resulting in increased power dissipation in the device. If the device junction temperature reaches the thermal shutdown threshold (T(TSD)), the internal FET is turn off. The device configured in latch-off mode stays latched off until it is reset by either of the following conditions:
Whereas the device configured in auto-retry mode, commences an auto-retry cycle 512 ms after TJ < [T(TSD) – 10°C]. The FLT signal remains asserted until the fault condition is removed and the device resumes normal operation. Figure 39 and Figure 40 illustrates behavior of the system during current limiting with auto-retry functionality.
Load transition from 22 Ω to 12 Ω | MODE pin connected to RTN | |
RILIM = 8 kΩ |
RILIM = 5.36 kΩ | ||