JAJSCF6G July 2016 – December 2019 TPS2660
PRODUCTION DATA.
During start-up, as the output capacitor charges, the voltage difference across the internal FET decreases, and the power dissipation decreases. Typical ramp-up of the output voltage, inrush current and instantaneous power dissipated in the device during start-up are shown in Figure 51. The average power dissipated in the device during start-up is equal to the area of triangular plot (red curve in Figure 52) averaged over tdVdT.
VIN = 24 V | CdVdT = 2.2 µF | COUT = 2.2 mF |
VIN = 24 V | CdVdT = 2.2 µF | COUT = 2.2 mF |
The inrush current is determined as shown in Equation 15.
Average power dissipated during start-up is given by Equation 16.
Equation 16 assumes that the load does not draw any current until the output voltage reaches its final value.