JAJSCO0D November 2016 – August 2021 LM5170-Q1
PRODUCTION DATA
One purpose of the peak current limit is to protect the power inductor from saturation. Select RIPK such that the peak current limit threshold is 5~10% greater than Ipeak. According to Equation 13, one gets:
Select RIPK = 40.2 kΩ, which results in a nominal inductor peak current limit of 44.2 A per channel.