JAJSDD8C July 2017 – June 2019 TLV743P
PRODUCTION DATA.
The TLV743P device uses a PMOS pass transistor to achieve low dropout. When (VIN – VOUT) is less than the dropout voltage (VDO), the PMOS pass device is in the linear region of operation and the input-to-output resistance is the RDS(ON) of the PMOS pass element. VDO scales approximately with output current because the PMOS device behaves like a resistor in dropout mode. As with any linear regulator, PSRR and transient response degrade as (VIN – VOUT) approaches dropout operation. See Figure 7 to Figure 12 for typical dropout values.