JAJSE45C February 2016 – December 2021 SN65DP141
PRODUCTION DATA
The SN65DP141 can be used in Source, Sink, cable, and dongle applications, where the device is transparent to the DisplayPort link layer. For illustrating purposes, this section shows the implementation of a DisplayPort dongle, Figure 9-1 shows an example of the SN65DP141 on a dongle board, where the AUX channel is directly connected from source to sink, meanwhile the power can be provided either way from the DP source or an external power source.