JAJSFO7D March 2008 – November 2023 UCC27324-Q1
PRODUCTION DATA
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | NC | — | No connection. Should be grounded. |
2 | INA | I | Input A. Input signal of the A driver. Has logic-compatible threshold and hysteresis. If not used, this input should be tied to either VDD or GND. It should not be left floating. |
3 | GND | — | Common ground. Should be connected very closely to the source of the power MOSFET that the driver is driving. |
4 | INB | I | Input B. Input signal of the B driver. Has logic-compatible threshold and hysteresis. If not used, this input should be tied to either VDD or GND. It should not be left floating. |
5 | OUTB | O | Driver output B. The output stage can provide 4-A drive current to the gate of a power MOSFET. |
6 | VDD | I | Supply. Supply voltage and the power input connection for this device. |
7 | OUTA | O | Driver output A. The output stage can provide 4-A drive current to the gate of a power MOSFET. |
8 | NC | — | No connection. Should be grounded. |