JAJSFQ3A July 2018 – September 2019 TPS56637
PRODUCTION DATA.
The TPS56637 has a built in discharge function by using an integrated MOSFET with 200-Ω RDS(on), which is connected to the output terminal SW. The discharge is slow due to the lower current capability of the MOSFET. The discharge path will be turned on when the device is turned off due to UV, OV, OT and EN shut down conditions.