JAJSG07E August 2012 – August 2018 LMZ21701
PRODUCTION DATA.
The output voltage of the LMZ21701 is set by a resistive divider from VOUT to GND, connected to the feedback (FB) pin. The output voltage can be set between 0.9 V and 6 V. The voltage at the FB pin is regulated to 0.8 V. The recommended minimum divider current is 2 μA. This sets a maximum limit on the bottom feedback resistor RFBB. Its value must not exceed 400 kΩ. The top feedback resistor RFBT can be calculated using the following formula: