JAJSHK9C June 2019 – September 2024 ADS7038
PRODUCTION DATA
In the on-the-fly mode of operation, the analog input channel is selected, as shown in Figure 7-15, using the first five bits on SDI without waiting for the CS rising edge. Thus, the ADC samples the newly selected channel on the CS rising edge and there is no latency between the channel selection and the ADC output data.
The number of clocks required for reading the output data depends on the device output data frame size; see the Output Data Format section for more details.