JAJSJ67E may 2020 – july 2023 UCC28782
PRODUCTION DATA
For secondary-resonance ACF, CO1 is used to adjust the resonant time with LK to fulfill the ZCS condition, so a large CCLAMP will not compromise ZCS. Besides, during the on-time of low-side switch (QL), the small CO1 is partially discharged by the load current at the same time. After QL turns off and the resonance begins, the discharged CO1 makes the initial resonance voltage lower than the reflected clamp capacitor voltage across CCLAMP, which forces more magnetizing current to be delivered to the output, so the conduction loss is reduced with less RMS current flowing through QH and the primary winding.