JAJSL17C October 2015 – February 2021 TPS61193
PRODUCTION DATA
The resistance of the input supply rail must be low enough so that the input current transient does not cause too high drop at TPS61193 VIN pin. If the input supply is connected by using long wires additional bulk capacitance may be required in addition to the ceramic bypass capacitors in the VIN line.