JAJSLJ8 March 2021 TPSM13604H
PRODUCTION DATA
None of the required output capacitance is contained within the module. At a minimum, the output capacitor must meet the worst-case RMS current rating of 0.5 × ILR P-P, as calculated in Equation 23. Beyond that, additional capacitance reduces output ripple so long as the ESR is low enough to permit it. A minimum value of 10 μF is generally required. Experimentation is required if the user is attempting to operate with a minimum value. Low-ESR capacitors, such as ceramic and polymer electrolytic capacitors, are recommended.