JAJSLL4C December 2016 – January 2021 HD3SS213
PRODUCTION DATA
Many interfaces require AC coupling between the source and sink. The 0402 capacitors are the preferred option to provide AC coupling, and the 0603 size capacitors also work. The 0805 size capacitors and C-packs must be avoided. When placing AC coupling capacitors symmetric placement is best. A capacitor value of 0.1 µF is best and the value must be match for the ± signal pair. There are several placement options for the AC coupling capacitors. Because the switch requires a bias voltage, the capacitors must only be placed on one side of the switch. If they are placed on both sides of the switch, a biasing voltage must be provided. A few placement options are shown below.
In Figure 8-1, the coupling capacitors are placed on the source pair. In this situation, the switch is biased by the sink.
In Figure 8-2, the coupling capacitors are placed between the switch and Sink. In this situation, the switch is biased by the Source