JAJSLU5B December 2021 – August 2024 TPS63901
PRODUCTION DATA
Figure 6-1 shows a simplified block diagram of the power stage of the device. Inductor current is sensed in series with Q1 (the peak current) and Q4 (the valley current).
The device uses a trapezoidal inductor current to regulate its output under all operating conditions. Thus, the device only has one operating mode and does not display any of the mode-change transients or unpredictable switching displayed by many other buck-boost devices.
There are four phases of operation:
Figure 6-2 shows the inductor current waveform when VI > VO, Figure 6-3 shows the current waveform when VI = VO, and Figure 6-4 shows the current waveform when VI < VO.
Figure 6-2 through Figure 6-4 show the typical waveforms during continuous conduction mode (CCM) switching for three operating conditions. During discontinuous conduction mode (DCM), the typical inductor current waveforms look similar to CCM with Phase D at 0-A inductor current. In deep boost mode, where VI << VO, Phase C length gradually decreases to zero until the switching waveform becomes triangular.
The ideal relationship between VI and VO (that is, assuming no losses) is:
where
By varying relative duration of each phase, the device can regulate VO to be less than, equal to, or greater than VI.