JAJSMA4A July 2021 – February 2022 LM74501-Q1
PRODUCTION DATA
For the LM74501-Q1 to operate in full conduction mode the gate driver must be enabled as described in the Gate Driver section. If these conditions are achieved, the GATE pin is internally connected to the VCAP pin, resulting in the GATE to SOURCE voltage being approximately the same as the VCAP to SOURCE voltage. By connecting VCAP to GATE, the external MOSFET is fully enhanced reducing the power loss of the external MOSFET.