JAJSNN2B October 2023 – July 2024 UCC25660
PRODUCTION DATA
UCC25660x ファミリ uses a multi-functional pin (OVP/OTP) that monitors for output overvoltage and external over-temperature conditions.
A Zener is connected between VCCP and the OVP/OTP pin. Under normal operating conditions, the Zener does not conduct and the OVP/OTP pin voltage is the result of the NTC resistance and IOTP source current. If VCCP rises high enough to exceed the Zener breakdown voltage, the voltage on the OVP/OTP pin is pulled high because of the Zener current. If the voltage on OVP/OTP exceeds the VOVPPos threshold for 40us the controller detects a fault and stops switching.
A NTC is connected from OVP/OTP to GNDP. An internal current source, IOTP, flows out of the OVP/OTP pin and into the NTC resistor. Based on the temperature of the NTC, the resulting voltage on the pin is compared to VOTPNeg to determine if an external over-temperature fault occurrs. Upon detection of external over-temperature protection, UCC25660x ファミリ moves to the fault state. After the 1-s wait period, UCC25660x ファミリ checks the OVP/OTP pin voltage. If the OVP/OTP pin voltage is higher than VOVPPos, the UCC25660x ファミリ attempts to restart, else it continues to wait in fault idle state. During burst mode, the over-temperature protection is disabled to minimize quiescent current. When transitioning from burst mode to normal switching, the OTP function is re-enabled.