JAJSQ80C september 2013 – october 2020 SN65DSI86
PRODUCTION DATA
The Generic Short Write with 2 parameters can be used for writing to SN65DSI86 CFR registers. The first parameter is the CFR Address and the second parameter is the data to be written to the address pointed to by the first parameter.
SOT | ID = 0x23 | ADDR (Byte) | DATA | ECC | EOT |
If GPU completes transmission with a BTA, the SN65DSI86 will respond with either an Acknowledge, if no errors were detected in current or previous packets, or an Acknowledge and Error Report packet, if errors were detected in current or previous packets.