JAJSS43 August 2024 AMC3306M25-Q1
PRODUCTION DATA
The AMC3306M25-Q1 is powered from the low-side power supply (VDD) with a nominal value of 3.3V or 5V. Place a low-ESR, 1nF decoupling capacitor (C8 in Figure 7-4) as close as possible to the VDD pin. Follow the 1nF capacitor with a 1µF capacitor (C9) to filter this power-supply path.
Decouple the low side of the DC/DC converter with a low-ESR, 100nF capacitor (C4) positioned close to the device between the DCDC_IN and DCDC_GND pins. Use a 1µF capacitor (C2) to decouple the high side. Additionally, place a low-ESR, 1nF capacitor (C3) as close as possible to the device and connect this capacitor to the DCDC_OUT and DCDC_HGND pins.
For the high-side LDO, use low-ESR, 1nF capacitors (C6), placed as close as possible to the AMC3306M25-Q1, followed by a 100nF decoupling capacitor (C5).
The ground reference for the high side (HGND) is derived from the terminal of the shunt resistor connected to the device negative input (INN). For best DC accuracy, use a separate trace to make this connection instead of shorting HGND to INN directly at the device input. The high-side DC/DC ground terminal (DCDC_HGND) is shorted to HGND directly at the device pins.
Make sure capacitors provide adequate effective capacitance under the applicable DC bias conditions experienced in the application. MLCC capacitors typically exhibit only a fraction of the nominal capacitance under real-world conditions; take this factor into consideration when selecting these capacitors. This problem is especially acute in low-profile capacitors, in which the dielectric field strength is higher than in taller components. Reputable capacitor manufacturers provide capacitance versus DC bias curves that greatly simplify component selection.
The Best Practices to Attenuate AMC3301 Family Radiated Emissions EMI application note is available for download at www.ti.com.
Table 7-2 lists recommended components for use with the AMC3306M25-Q1. This list is not exhaustive. Other components potentially exist that are equally capable (or better), however these listed components have been validated during the development of the AMC3306M25-Q1.
DESCRIPTION | PART NUMBER | MANUFACTURER | SIZE (EIA, L × W) | |
---|---|---|---|---|
VDD | ||||
C8 | 1nF ± 10%, X7R, 50V | 12065C102KAT2A(1) | AVX | 1206, 3.2mm × 1.6mm |
C0603C102K5RACTU | Kemet | 0603, 1.6mm × 0.8mm | ||
C9 | 1µF ± 10%, X7R, 25V | 12063C105KAT2A(1) | AVX | 1206, 3.2mm × 1.6mm |
CGA3E1X7R1E105K080AC | TDK | 0603, 1.6mm × 0.8mm | ||
DC/DC CONVERTER | ||||
C4 | 100nF ± 10%, X7R, 50V | C0603C104K5RACAUTO | Kemet | 0603, 1.6mm × 0.8mm |
C3 | 1nF ± 10%, X7R, 50V | C0603C102K5RACTU | Kemet | 0603, 1.6mm × 0.8mm |
C2 | 1µF ± 10%, X7R, 25V | CGA3E1X7R1E105K080AC | TDK | 0603, 1.6mm × 0.8mm |
HLDO | ||||
C1 | 100nF ± 10%, X7R, 50V | C0603C104K5RACAUTO | Kemet | 0603, 1.6mm × 0.8mm |
C5 | 100nF ± 5%, NP0, 50V | C3216NP01H104J160AA(1) | TDK | 1206, 3.2mm × 1.6mm |
100nF ± 10%, X7R, 50V | C0603C104K5RACAUTO | Kemet | 0603, 1.6mm × 0.8mm | |
C6 | 1nF ± 10%, X7R, 50V | 12065C102KAT2A(1) | AVX | 1206, 3.2mm × 1.6mm |
C0603C102K5RACTU | Kemet | 0603, 1.6mm × 0.8mm | ||
FERRITE BEADS | ||||
FB1,FB2, FB3 | Ferrite bead(2) | 74269244182 | Wurth Elektronik | 0402, 1.0mm × 0.5mm |
BLM15HD182SH1 | Murata | 0402, 1.0mm × 0.5mm | ||
BKH1005LM182-T | Taiyo Yuden | 0402, 1.0mm × 0.5mm |