JAJSUN1A May 2024 – September 2024 TPS7H1121-SP
PRODMIX
To determine the overall output voltage accuracy, refer to the device voltage accuracy VACC from the Section 6.5, the top and bottom feedback resistors (RFB(Top) and RFB(BOT)).
When the input voltage VIN is below 3V, the error amp is operating with a reduced head room such that output accuracy performance is widened to ±1.8%; for this example VIN is above 3V, therefore the standard ±1.5% accuracy can be applied.
For the selected 0.1% feedback resistors, the calculated error is shown in Equation 8, this assumes an uncorrelated error and the errors are added as the sum of the resistors' error squared.
The negative and positive system error's are summed with the results for this example shown below in equations Equation 9 and Equation 10.
Adding the following errors together results in an accuracy of ±1.64%.