JAJSVF9 September 2024 TSD5402-Q1
PRODUCTION DATA
When using a single-ended signal source, ac-ground the negative input through a capacitor equal in value to the input capacitor on the positive input, and apply the signal source to the positive input. For best performance, the ac ground should be at the signal source instead of at the device input if possible.