JAJU787B April   2016  – May 2019 TPS2828 , TPS3828

 

  1.   改訂履歴

Flashing Hybrid RF/PLC Example Binary to CC1310 Using CCS

This section covers how to flash the Hybrid RF/PLC example binary on the CC1310 using CCS.

  1. Connect the USB cable to LAUNCHXL-CC1310 EVM..
  2. Launch the target configuration for CC1310 and connect to the device in hte CCS debug mode.
  3. Select Run → Load → Load Program and flash the "HybridRfPlcExample_CC1310_LAUNCHXL_tirtos_ccs.out" binary in the directory of debug.