JAJU788A June   2016  – May 2019 TPS3828

 

  1.   改訂履歴

PLC Only Node Setup

This section covers how to run the PLC only node as a mini-DC with GUI.

  1. Connect the PLC only node to the PC and open the intermediate GUI.
  2. Set a unique long address for each device by using Set System Config.
  3. Figure 17. Set System ConfigurationTIDC-HYBRID-WMBUS-PLC Fig_19_Set_Sys_Config_TIDUBS4.gif
    Figure 18. G3-PLC System ConfigurationTIDC-HYBRID-WMBUS-PLC Fig_20_G3PLC_Sys_Config_TIDUBS4.gif
  4. Start a device as a mini-DC by selecting Functions → Start Base Node.
  5. Figure 19. Start Base NodeTIDC-HYBRID-WMBUS-PLC Fig_21_Start_Base_Node_TIDUBS4.gif
  6. In the pop-up window of the G3 Base Node, click Start Network.
  7. Figure 20. G3-PLC Base Node WindowTIDC-HYBRID-WMBUS-PLC Fig_22_G33PLC_Base_Node_TIDUBS4.gif
  8. Once the hybrid wireless M-Bus/PLC node is joined, the IPv6 information for the joined node will be available.
  9. Figure 21. Joining Node InformationTIDC-HYBRID-WMBUS-PLC Fig_23_Joining_Node_TIDUBS4.gif
  10. Set the Max Data Packet Size to 184 due to the maximum size limitation of the wireless M-Bus specification. Then, start data echo-back testing by selecting Start Test.
  11. Figure 22. Start Data Echo-Back TestTIDC-HYBRID-WMBUS-PLC Fig_24_Start_Data_TIDUBS4.gif