JAJU835 December 2021
When the external magnet was applied to the trigger module according to the orientation shown in Figure 2-11, the system did not turn ON. The external magnet caused the output of the wake-up sensor to be asserted low due to the sensor detecting a strong positive field; however, the system remained OFF since the external magnet caused the stray field sensor to also detect a strong positive field instead of the negative field needed to turn the system ON.
The external magnet was also applied to the trigger module according to the orientation shown in Figure 2-12. In this orientation, the output of both the wake-up and stray field sensor was asserted low, but the system did not turn ON due to either U3 or U4 detecting this external magnetic field.