SBAA378B November 2019 – December 2023 PCM3140-Q1 , PCM5140-Q1 , PCM6140-Q1 , TLV320ADC3140 , TLV320ADC5140 , TLV320ADC6140
Figure 3-2 shows how to create a set of filters for 5-dB boost at 500 Hz with bandwidth of 400 Hz, cut –5 dB at 2 kHz with 3-kHz bandwidth, and a Notch filter at 60 Hz with 50-Hz bandwidth for channel 1. Note that each biquad filter is color coded. The cyan color refers to BQ1 500-Hz equalizer, light gray to BQ5 2 kHz, and brown to BQ9 Notch filter at 60 Hz. The overall response of all three filters is plotted in red. Note that cutoff or center frequencies are marked on the graph to allow you to drag and move the center frequencies of the filters. The graphical plots allows users to zoom in and out of the frequency response plot and choose logarithmic or linear frequency axis, plot gain, phase, group delay, or impulse response.
Clicking on the swivel arrow at each biquad shows the normalized floating point coefficients for N0, N1, N2, D1, and D2 of Equation 3, as shown in Figure 3-3. Note the PurePath Console has computed the floating point coefficients b0, b1, b2, a1, and a2 of Equation 2 and converted into the necessary values for N0, N1, N2, D1, and D2. Clicking the Apply button transmits the coefficients through I2C to the TLV320ADCx140/PCMx140-Q1 devices on the EVM.