In modern highly-integrated digital systems for data acquisition, high-speed analog-to-digital converters (ADCs) play a major role in transforming signals into their digital representation. As ADCs are a vital component of the overall system signal chain of wireless communications, electronic warfare, radar systems, medical imaging, and other applications, they must perform effectively to maintain a high spurious-free dynamic range (SFDR), establishing a distinguishable signal from noise. Therefore, ADC calibration is of utmost importance to improving SFDR by reducing noise and enhancing signal distinguishability. Specifically, calibration reduces errors, consequently allowing for SFDR improvement. This application note discusses different approaches for ADC calibration commonly found in most modern converters, including one-time calibration, background calibration, and foreground calibration.
All trademarks are the property of their respective owners.
High-speed ADCs play a crucial role in modern highly-integrated digital systems; however, these ADCs are prone to introducing a range of errors, which significantly impacts the accuracy of the sampled signal. Among these errors are gain errors, offset errors, and linearity deviations, which cause distortion of the obtained data. Fortunately, calibration can effectively minimize these errors and enhance the performance of the ADC, bringing it closer to the expected behavior.
Calibration has become an essential aspect of modern ADC designs, driven by the adoption of more advanced process nodes (such as 0.18 μm or smaller). These process nodes allow for additional digital feature integration within the ADC architecture. By introducing serial registers to enable or disable specific features, the concept of digital trimming emerged as a replacement for the traditional method of laser trimming the bias currents of a device for improved INL and linearity.
Reflecting on the past when laser trimming of internal ADC bias currents was the norm, the ADC performance of the ADC was fixed at the highest speed or sampling rate for which it was trimmed. Any deviation from this intended sample rate resulted in compromised performance. This limitation drove the push towards multiple speed grades of a device within an ADC device family, catering towards different sampling rate requirements.
As technology advanced further, reaching 65 nm and below, the space for digital features on a data converter has grown significantly, enabling the incorporation of more digital components and features. This expansion opens up new possibilities for real-time calibration and allows for dynamic trimming of the ADC.
Real-time calibration has become the standard approach for linearizing ADC performance at various sample rates and input frequencies. These calibration methods act to provide flexibility to system designers, allowing for a tailored ADC performance in their specific application. By providing a seemingly unlimited amount of flexibility, calibration enables the system designer to achieve optimal performance regardless of the variation in sampling rate or input frequency (a significant advancement over laser trimming). As a result, the same ADC delivers excellent performance across many different applications, enabling reconfigurable systems.
Several factors can contribute to the degradation or loss of calibration in a high-speed ADC. These factors can affect the accuracy and performance target of the ADC, leading to a point where re-calibration is necessary. The following section discuss some common factors that can cause a high-speed ADC to become uncalibrated.