SBAA590 june   2023 ADC12DJ5200RF , ADC32RF52 , ADC32RF54 , ADC32RF55 , ADC34RF52 , ADC34RF55

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Achieving Accuracy Through Calibration
    1. 2.1 Temperature Variations
    2. 2.2 External Noise
    3. 2.3 Unstable Power Supply
    4. 2.4 Mechanical Stress
    5. 2.5 Manufacturing Variations
    6. 2.6 Avoiding Errors
  6. 3Calibration Techniques
    1. 3.1 One-Time Calibration
    2. 3.2 Foreground Calibration
    3. 3.3 Background Calibration
  7. 4Summary
  8. 5References

One-Time Calibration

The process of one-time calibration involves performing calibration only once during the initial bring-up sequence of the data converter. In the specific case of the ADC32RF55, a dual-channel, 14-bit, 3 GSPS RF-sampling ADC, the initial bring-up sequence is performed to calibrate all of the internal sub-ADC cores, allowing for data sheet performance to be realized. Without performing this one-time calibration, the converter is severely degraded and there is no worthwhile data to be processed as shown in Figure 3-1. However, after this one-time calibration, the FFT is as expected as shown in Figure 3-2.

GUID-20230601-SS0I-CZ2P-HCCM-3FJ5P7L0C5VL-low.png Figure 3-1 ADC32RF55 Output Without One-time Calibration
GUID-20230601-SS0I-B6ST-BWKS-75WG3BXXTSLW-low.png Figure 3-2 ADC32RF55 Output With One-time Calibration

Similarly, the ADC12DJ5200RF, a dual-channel, 12-bit, 5.2GSPS RF-sampling ADC, also requires a one-time calibration such, that the gain and the offset of the sub-ADC cores are matched, thereby reducing interleaving spurs and improving SFDR. One-time calibration is performed by the serial peripheral interface (SPI) during the initial programming of both the ADC32RF55 and the ADC12DJ5200RF devices.