SBAU336A March 2020 – March 2021 AMC3306M05 , AMC3306M25 , AMC3336 , AMC3336-Q1
After the VDD power and the external clock input at CLKIN are applied to the AMC33xxEVM, the DOUT pin will begin to generate a bitstream output.
An analog input signal may be applied directly at screw terminal J2. See Figure 2-1 and Table 4-1 for details. For the AMC3306EVM, the differential analog input range, (VIN+) – (VIN–), is specified at ±250 mV with a maximum of ±320 mV before clipping occurs. For the AMC3336EVM, the differential analog input range, (VIN+) – (VIN–), is specified at ±1 V with a maximum of ±1.25 V before clipping occurs.
The digital output is a bitstream that alternates between 0 V and VDD. Using the AMC3306 for example, a differential input signal of 0 V ideally produces a stream of ones and zeros that are high 50% of the time, while a differential input of 250 mV produces a bitstream that is high 89.06% of the time. If the input is less than –320 mV or greater than 320 mV, the output modulator clips with a stream of only zeros or ones. In this case, however, the AMC3306 generates a single one or zero every 128 clock cycles to indicate proper device function.