SBAU390A September 2021 – April 2024 TMAG5170 , TMAG5170-Q1 , TMAG5173-Q1 , TMAG5273
This SLIDEBY-MAG-ACC attachment uses an N42 grade cylindrical magnet as a magnetic field source to demonstrate the ability of magnetic sensors to track linear motion of a nearby magnet. The magnet is glued into the slider object, which then can pass freely down the length of the slider track. Slider options for both a vertically aligned or horizontally aligned magnet are included in the EVM kit. More details about this function are described in Tracking Slide-By Displacement with Linear Hall-Effect Sensors.
Examples of expected magnetic field data captured using the TMAG5170UEVM are shown in Figure 1-1 and Figure 1-2.
Nylon components were selected as these components are non-magnetic and do not interfere with the magnetic field and bond well when glued.
This function can be further explored using the slide-by reference design in the TI Magnetic Sense Simulator tool (TIMSS) available at https://webench.ti.com/timss/.